i.mx53 Sabre WinCE7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 Sabre WinCE7

1,071件の閲覧回数
GuillermoHernan
Contributor III

Question 1
we are using the imx53 SABRE AI REV.B2 board and we choose the windows embedded compact 7 system.
we use the latest windows embedded compact 7(to update 7). build the nk.bin,downloading the os, but after we attach device, the terminal(serial port ) print the flowing error message:  
INFO: OEMMultiBINNotify (dwNumRegions = 1, dwRegionStart = 0x9fa80400).
INFO: OEMVerifyMemory (CA = 0x9fa80400, PAStart = 0xf8080400, PAEnd = 0xfc058247, length = 0x3fd7e48)
INFO: Downloading NK SD/MMC image.
!CheckUDP: UDP header checksum failure
!CheckUDP: UDP header checksum failure
!CheckUDP: UDP header checksum failure
!CheckUDP: UDP header checksum failure
!CheckUDP: UDP header checksum failure
!CheckUDP: UDP header checksum failure
 the bsp we download modified at:1/16/2012 by yours.
would you tell me how to solve the problem?

Question 2
we choose the silverlight graphical shells ,select the silverlight themes after sysgen and build, the graphical shell can not load suceessful and the graphics can not appears

 

Answers:

 

For issue 1:
this is a known behaviour, you can just ignore it as it should not represent any performance issue, some people have reported to get if off it by plugging a usb storage device and unplugging it, but this is not officially supported.

for issue 2:
Silverlight requieres licensing, thus it can not be built using the BSP, the demo image however has it embedded along with a sample app

タグ(2)
0 件の賞賛
返信
0 返答(返信)