i.mx53 CSI issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 CSI issues

1,619 Views
aworthi
Contributor II

We’re running into a complicated problem with the i.MX53 CSI port. We’ve changed from bringing in single still images to streaming video for a particular project and the frame rate he sees is half the frame rate the imager is putting out. We’re trying to trace it down here, but we’re not sure if it’s something not getting set up correctly in the driver or what. Are there any known problem with the driver or something.

We have looked further into the problem and it’s a hard one to solve. We’ve modified the software to dump more diagnostic info and I modified the FPGA that routes the data from the VITA2000 imager to the CSI port to generate a start of frame (SOF) interrupt to the i.MX53. We definitely see two SOFs for every frame the i.MX53 sees. We’ve looked at the config registers in the CSI and they are not set to bring in interlaces video. So, it must be some kind of frame skipping mechanism getting turned on somewhere.

0 Kudos
Reply
1 Reply

1,473 Views
igorpadykov
NXP Employee
NXP Employee

Hi aworthi

one can check if timings are correct with

sect.4.7.7.1 IPU Sensor Interface Signal Mapping,

sect.4.7.7.2 Sensor Interface Timings IMX53CEC

also links below may be helpful

MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?

Re: Blurry image with CSI1 overlay

OBDS (camera example) may be useful for hardware bring-up

On-Board Diagnostic Suit for the i.MX53 Quick Start Board

Best regards

igor

0 Kudos
Reply