i.mx28 wrong battery voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx28 wrong battery voltage

1,384 次查看
sinan
Contributor I

Hi all,

I need to get battery voltage, but both of "/sys/class/power_supply/battery/uevent" and HW_POWER_BATTMONITOR.BATT_VAL bits have wrong values (~4200mV). Also when the battery is disconnected (and it reboots), it is still appears that battery is present.

Any answer will be appreciated.

Regards,

Sinan

标记 (2)
0 项奖励
回复
1 回复

1,213 次查看
Yuri
NXP Employee
NXP Employee

   Please check if Your schematic (regarding battery using) is the same as the i.MX28 EVK.

Also, please verify if corresponding software (driver) configured correctly.
Driver details may be found in Chapter 27 [Battery Charger and Power Source Manager
(PSM) Driver] of "MX28_EVK_Linux_Reference_Manual.pdf".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复