i.mx28 NAND flash programming using JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28 NAND flash programming using JTAG

1,843 Views
SteveO1z
Contributor II

Hello. I have been asked if it is possible to program the NAND flash using JTAG in a manufacturing environment. We are using an i.mx28 with a NAND flash connected through the GPMI. Has anyone had experience with this process? Is this practical in a MFG environment? We have maintained the standard 8-pin connector from the SDK. Any suggestions on tools or known issues would be greatly appreciated. Thanks in advance!

Steve O

Labels (1)
0 Kudos
Reply
1 Reply

1,626 Views
igorpadykov
NXP Employee
NXP Employee

Hi Steve

typical option is to use mfg tools for nand programming

Programmers (Flash, etc.) (6)

i.MX287 Processors|Dual Ethernet|NXP 

unfortunately I am not aware of jtag programming options.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply