i.mx 6solox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx 6solox

1,531 次查看
feitang
Contributor I

I have two flash,  "NOR Flash (MT25QL128ABA8E12-0)"&"NAND Flash (MT29F1G08ABAEAH4)".

I want use JTAG interface to flashing data into NOR&NAND through i.mx 6solox ,use "PE cycloneuniversal" programmer.

I want to know ,if this programmer can satisfy  the demands ,and how do i need to do.

标签 (1)
0 项奖励
回复
1 回复

1,471 次查看
igorpadykov
NXP Employee
NXP Employee

Hi fei

for programming images to external media may be used mfg tool or uuu described on link

i.MX Software | NXP 

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

unfortunately programming using "PE cycloneuniversal" is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复