i.Mx6d Android board lvds panel display problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx6d Android board lvds panel display problem

1,669件の閲覧回数
261799945
Contributor I

I have a i.mx6d borad, and i transplant Android4.3 system to it,  the display panel is lvds 1024*768 60HZ, it goes very ok when it power on, but after 10minutes, the display screen occur overlays. see the image.   it seems something wrong with the ipu or the ldb driver, so i do modify the ldb drivers but the problem still the same , can anyone give some advise? Very thanks if get answers.

Picture 1: power on desktop,is ok

ok.jpg

Picture 2: after several minutes it change like this

bad.jpg

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,615件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

It seems the display output is normal after boot up.

Please double check the connection (cable?) between the display and your board.  Maybe the signals are not stable.

0 件の賞賛
返信

1,615件の閲覧回数
261799945
Contributor I

Thanks for answer, i have use another cable to connect it , but the problem still the same, maybe it is the display problem, i will test it with a new 

display.

0 件の賞賛
返信