i.Mx6d Android board lvds panel display problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx6d Android board lvds panel display problem

1,659 Views
261799945
Contributor I

I have a i.mx6d borad, and i transplant Android4.3 system to it,  the display panel is lvds 1024*768 60HZ, it goes very ok when it power on, but after 10minutes, the display screen occur overlays. see the image.   it seems something wrong with the ipu or the ldb driver, so i do modify the ldb drivers but the problem still the same , can anyone give some advise? Very thanks if get answers.

Picture 1: power on desktop,is ok

ok.jpg

Picture 2: after several minutes it change like this

bad.jpg

Labels (2)
0 Kudos
Reply
2 Replies

1,605 Views
jimmychan
NXP TechSupport
NXP TechSupport

It seems the display output is normal after boot up.

Please double check the connection (cable?) between the display and your board.  Maybe the signals are not stable.

0 Kudos
Reply

1,605 Views
261799945
Contributor I

Thanks for answer, i have use another cable to connect it , but the problem still the same, maybe it is the display problem, i will test it with a new 

display.

0 Kudos
Reply