i.Mx6Q frame buffer 2 issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.Mx6Q frame buffer 2 issue

2,969 次查看
daonamthai
Contributor I

Hello everyone,

I got some issues with fb2.

Step 1: Show ring buffer infomation about mxc

dmesg | grep mxc_sdc

output:

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver lcd

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver hdmi

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb

that mean hdmi is port is mapped to frame buffer 1

Step 2: Show frame buffer infor

cat /sys/class/graphics/fb1/modes

Output:

U:240x320p-60

Maybe, it's strange

I also checkout fb2 mode

cat /sys/class/graphics/fb2/modes

Output:

V:1280x1024p-60

V:1024x768p-60

U:1280x720p-120

U:1280x720p-100

U:1920x1080p-30

U:1920x1080p-25

U:1920x1080p-24

U:1920x1080p-50

U:1440x576p-50

U:1440x576p-50

U:1440x288p-50

U:1440x288p-50

U:1280x720p-50

U:720x576p-50

U:720x576p-50

U:1920x1080p-60

U:1440x480p-60

U:1440x480p-60

U:1440x240p-60

U:1440x240p-60

U:1280x720p-60

U:720x480p-60

U:720x480p-60

U:640x480p-60

I guess fb2 is frame buffer for hdmi port

Step 3: I rebuild fb-test app to test frame buffer

fb 0 worked well. We can display image on LCD and DVI port at the same time.(DVI and LCD use IPU1_DISP0)

fb 1 or 2 did not work. No thing displayed on screen

Test procedure

export DISPLAY=:2                                    //(or 0,1) export fb to user space ???

echo 0>/sys/class/graphics/fb2/blank          //unblank screen

./fb-test 2                                                     //run test application with fb2

My system

uname -a

Linux devel 3.0.35 #805 SMP Thu Apr 24 17:12:39 IDT 2014 armv7l GNU/Linux

what's is wrong in here?

Thank all,

Thaidao

标签 (4)
0 项奖励
回复
2 回复数

1,972 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I would like to test the same application and debug the issue. Can you tell me where I can get it?

Alejandro

0 项奖励
回复

1,972 次查看
daonamthai
Contributor I

Hi,

I followed this link to study frame buffer:

OpenEmbedded/Video_Out – Gateworks.

Then, you can install git and download source code by below link

https://github.com/prpplague/fb-test-app

You must change makefile configuration depend on your host system.

Note: Makefile will create some applications in sample time.

Sincerely,

Thaidao

0 项奖励
回复