i.MX8m Mini EVK USB1 vs USB2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8m Mini EVK USB1 vs USB2

1,310 Views
faiz
Contributor I

Hello,

On the i.MX8m mini evk, USB1 (J301) is the download port while USB2 (J302) is the power supply port. Looking at the schematic (Page 6), both USB1 and USB2 appear to have similar design except, on USB1, EN_SNK1 (U303) is not directly connected to 3483_EN_SNK1(U302). It goes through this circuit:

pastedImage_2.png

On our application, we only need USB1 to download firmware and we are doing something else for power. 

1) Are EN_SNK1 (U303) and 3483_EN_SNK1(U302) the only thing from preventing USB1 from acting as power supply port?

2) If we just need USB1 for downloading firmware, can I just leave EN_SNK1 (U303) and 3483_EN_SNK1(U302) pins open?

Thank you,
Faiz

0 Kudos
Reply
1 Reply

1,230 Views
art
NXP Employee
NXP Employee

Q. Are EN_SNK1 (U303) and 3483_EN_SNK1(U302) the only thing from preventing USB1 from acting as power supply port?

A. Yes.

Q. If we just need USB1 for downloading firmware, can I just leave EN_SNK1 (U303) and 3483_EN_SNK1(U302) pins open?

A. You can leave EN_SNK1 (U303) open and tie 3483_EN_SNK1(U302) to GND.

Have a great day,

Artur

0 Kudos
Reply