i.MX8QXP M4 config GPIO question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP M4 config GPIO question

1,580 Views
xu_ji1
Contributor V

Hello,

      I need use some pins as LSIO function in M4 side,pin "SC_P_QSPI0A_SCLK  SC_P_ENET0_RGMII_TX_CTL  SC_P_ENET0_RGMII_RXC  SC_P_SPI3_CS0", I set this pads and resource to M4 side in SCFW and init GPIO used

GPIO_PinInit() function,but when I used GPIO_WritePinOutput() function pullup GPIO in driver,test the GPIO current,it is have no changed.

      Does M4 side can control LSIO GPIO?or only can control M40_GPIO?

Thanks

0 Kudos
Reply
2 Replies

1,439 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Xu,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply

1,439 Views
xu_ji1
Contributor V

Hello,

i.MX8 ga release now,also can not anwser my question?

Thanks

0 Kudos
Reply