i.MX8QXP C0 MEK; 'USB Root Hub' device does not appear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP C0 MEK; 'USB Root Hub' device does not appear

1,183 Views
ellabyoon
Contributor I

I bought a i.MX8QXP MEK evaluation board from NXP.
I fused the image provided by NXP and am testing USB related functions.
It is using the kernel, DTB, and root filesystem as provided by NXP, but there are a few problems:

A. The 'USB Root Hub' device does not appear

On my i.MX8M Mini Board, with no USB device connected, I get this message:

# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

However, no message is displayed on the MEK board.

B. modprobe g_ether

An error message appears when loading the USB Gadget driver.
Modules are loaded, but Ethernet devices such as usb0 do not appear.

root@imx8qxpc0mek:~# modprobe g_ether
[ 1929.547702] udc-core: couldn't find an available UDC - added [g_ether] to list of pending drivers

 

Environment:

-Linux Kernel 5.15.52+g36363d8623ba
-imx8qxp-mek.dtb

root@imx8qxpc0mek:~# uname -a
Linux imx8qxpc0mek 5.15.52+g36363d8623ba #1 SMP PREEMPT Tue Sep 6 09:50:50 UTC 2022 aarch64 GNU/Linux


We really need your help.

Tags (2)
0 Kudos
Reply
0 Replies