i.MX8QM display problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QM display problem

2,173件の閲覧回数
cptb
Contributor I

I encountered the problem of screen probability performance lighting, hope someone can help solve, using i.MX8QM development board and RM67191 screen. When I burned the Android tablet image, the screen was normal and could be lit up 100%. When I burned the car image, the screen was lit up with probability and the display image was rotated 90 degrees. The car image should have used two switching boards, lvds-to-hdmi and mipi-to-hdmi. I removed the adapter board driver and device tree directly using the mipi screen display. Attempts to modify the screen parameters and modify the rotation parameter of drm_plane did not solve the problem.

[    8.453102][  T236] random: init: uninitialized urandom read (40 bytes read)
[    8.483181][  T236] random: init: uninitialized urandom read (40 bytes read)
[    8.490710][  T236] random: init: uninitialized urandom read (4 bytes read)
[    8.598901][  T237] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.
v33: No such file or directory
[    8.610362][  T237] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.
v33: No such file or directory
[    8.625025][  T237] linkerconfig (237) used greatest stack depth: 11112 bytes left
[    8.668069][  T238] ueventd: ueventd started!
[    8.675794][  T238] selinux: SELinux: Loaded file_contexts
[    8.681342][  T238] selinux: 
[    8.685456][  T238] ueventd: Parsing file /system/etc/ueventd.rc...
[    8.691919][  T238] ueventd: Added '/vendor/etc/ueventd.rc' to import list
[    8.698849][  T238] ueventd: Added '/odm/etc/ueventd.rc' to import list
[    8.705987][  T238] ueventd: Parsing file /vendor/etc/ueventd.rc...
[    8.711027][  T239] apexd: Bootstrap subcommand detected
[    8.713159][  T238] ueventd: /vendor/etc/ueventd.rc: 42: /sys/ lines must have 5 or 6 entries
[    8.717683][  T239] apexd: ActivateFlattenedApex
[    8.726366][  T238] ueventd: Parsing file /odm/etc/ueventd.rc...
[    8.730900][  T239] apexd: Scanning /system/apex
[    8.736861][  T238] ueventd: Unable to read config file '/odm/etc/ueventd.rc': open() failed:
 No such file or directory
[    8.741956][  T239] apexd: Bind mounting /system/apex/com.android.adbd onto /apex/com.android
.adbd
[    8.762248][  T239] apexd: Bind mounting /system/apex/com.android.adservices onto /apex/com.a
ndroid.adservices
[    8.773021][  T239] apexd: Bind mounting /system/apex/com.android.appsearch onto /apex/com.an
droid.appsearch
[    8.783619][  T239] apexd: Bind mounting /system/apex/com.android.art onto /apex/com.android.
art
[    8.793930][  T239] apexd: Bind mounting /system/apex/com.android.btservices onto /apex/com.a
ndroid.btservices
[    8.804962][  T239] apexd: Bind mounting /system/apex/com.android.car.framework onto /apex/co
m.android.car.framework
[    8.816344][  T239] apexd: Bind mounting /system/apex/com.android.cellbroadcast onto /apex/co
m.android.cellbroadcast
[    8.854382][  T239] printk: apexd: 26 output lines suppressed due to ratelimiting
[    9.097141][  T241] <unknown>: getrandom indicates that the entropy pool has not been initial
ized. Rather than continue with poor entropy, this process will block until entropy is available
.
[    9.658561][    C1] random: crng init done
[    9.662687][    C1] random: 38 urandom warning(s) missed due to ratelimiting
[    9.720426][  T241] boringssl_self_ (241) used greatest stack depth: 10992 bytes left
[    9.821188][  T249] boringssl_self_ (249) used greatest stack depth: 10968 bytes left
[    9.871181][   T58] audit: type=1400 audit(1689388936.796:4): avc:  denied  { sys_admin } for
  pid=250 comm="init.insmod.sh" capability=21  scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-
insmod-sh:s0 tclass=capability permissive=0
[    9.917814][  T253] setprop (253) used greatest stack depth: 10816 bytes left
[   10.085073][  T256] module built by bfz at 2023年 07月 17日 星期一 10:09:47 CST
[   10.087489][  T256] Galcore version 6.4.3.p4.398061
[   10.121825][  T256] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu1_ss on min
or 0
[   10.122752][    T1] Registered swp emulation handler
[   10.166813][  T251] binder: 251:251 transaction failed 29189/-22, size 0-0 line 2920
[   10.199529][  T260] Hot alarm is canceled. GPU3D clock will return to 64/64
[   10.213003][  T261] logd.auditd: start
[   10.217328][  T261] logd.klogd: 10118762375
[   10.228145][  T271] watchdogd: watchdogd started (interval 10, margin 20)!
mek_8q:/ $ [   10.253153][  T261] logd: Loaded bug_map file: /vendor/etc/selinux/selinux_denial_
metadata
[   10.262805][  T261] logd: Loaded bug_map file: /system/etc/selinux/bug_map
[   10.620001][  T298] send message failed!
[   10.624301][  T298] send message failed!
[   10.628526][  T298] send message failed!
[   10.632730][  T298] send message failed!
[   10.636873][  T298] send message failed!
[   10.641059][  T298] send message failed!
[   10.645209][  T298] send message failed!
[   10.649352][  T298] send message failed!
[   10.653455][  T298] send message failed!
[   10.657554][  T298] send message failed!
[   10.661698][  T298] send message failed!
[   10.665948][  T298] send message failed!
[   10.670116][  T298] send message failed!
[   10.674285][  T298] send message failed!
[   10.678423][  T298] send message failed!
[   10.682627][  T298] send message failed!
[   10.686805][  T298] send message failed!
[   10.691204][  T298] send message failed!
[   10.695497][  T298] send message failed!
[   10.699650][  T298] send message failed!
[   10.703796][  T298] send message failed!
[   10.707926][  T298] send message failed!
[   10.712172][  T298] send message failed!
[   10.716422][  T298] send message failed!
[   10.720547][  T298] send message failed!
[   10.724729][  T298] send message failed!
[   10.729025][  T298] send message failed!
[   10.733075][  T298] send message failed!
[   10.737118][  T298] send message failed!
[   10.741202][  T298] send message failed!
[   10.745246][  T298] send message failed!
[   10.749290][  T298] send message failed!
[   10.753313][  T298] send message failed!
[   10.757366][  T298] send message failed!
[   10.761423][  T298] send message failed!
[   10.765455][  T298] send message failed!
[   10.769026][  T277] fsck.f2fs: Info: Fix the reported corruption.
[   10.769482][  T298] send message failed!
[   10.775597][  T277] fsck.f2fs: Info: not exist /proc/version!
[   10.779560][  T298] send message failed!
[   10.785289][  T277] fsck.f2fs: Info: Segments per section = 1
[   10.789339][  T298] send message failed!
[   10.795049][  T277] fsck.f2fs: Info: Sections per zone = 1
[   10.799060][  T298] send message failed!
[   10.804833][  T277] fsck.f2fs: Info: sector size = 4096
[   10.808571][  T298] send message failed!
[   10.813817][  T277] fsck.f2fs: Info: total sectors = 2257408 (8818 MB)
[   10.817838][  T298] send message failed!
[   10.824357][  T277] fsck.f2fs: Info: MKFS version
[   10.828377][  T298] send message failed!
[   10.833074][  T277] fsck.f2fs:   "5.15.71-g279b46e22312-dirty"
[   10.837093][  T298] send message failed!
[   10.842972][  T277] fsck.f2fs: Info: FSCK version
[   10.846909][  T298] send message failed!
[   10.851598][  T277] fsck.f2fs:   from "5.15.71-g279b46e22312-dirty"
[   10.855531][  T298] send message failed!
[   10.865951][  T298] send message failed!
[   10.870004][  T298] send message failed!
[   10.874091][  T298] send message failed!
[   10.878158][  T298] send message failed!
[   10.882234][  T298] send message failed!
[   10.886324][  T298] send message failed!
[   10.890354][  T298] send message failed!
[   10.894422][  T298] send message failed!
[   10.899099][  T298] send message failed!
[   10.903295][  T298] send message failed!
[   10.907334][  T298] send message failed!
[   10.911392][  T298] send message failed!
[   10.915373][  T298] send message failed!
[   10.919392][  T298] send message failed!
[   10.923473][  T298] send message failed!
[   10.927534][  T298] send message failed!
[   10.931573][  T298] send message failed!
[   10.935603][  T298] send message failed!
[   10.939667][  T298] send message failed!
[   10.943742][  T298] send message failed!
[   10.947821][  T298] send message failed!
[   10.951911][  T298] send message failed!
[   10.955995][  T298] send message failed!
[   10.960080][  T298] send message failed!
[   10.964222][  T298] send message failed!
[   10.968294][  T298] send message failed!
[   10.972387][  T298] send message failed!
[   10.976434][  T298] send message failed!
[   10.980526][  T298] send message failed!
[   10.984586][  T298] send message failed!
[   10.988709][  T298] send message failed!
[   10.992825][  T298] send message failed!
[   10.996952][  T298] send message failed!
[   11.001023][  T298] send message failed!
[   11.005102][  T298] send message failed!
[   11.009189][  T298] send message failed!
[   11.013275][  T298] send message failed!
[   11.017370][  T298] send message failed!
[   11.021590][  T298] send message failed!
[   11.025621][  T298] send message failed!
[   11.029664][  T298] send message failed!
[   11.033646][  T298] send message failed!
[   11.037632][  T298] send message failed!
[   11.041604][  T298] send message failed!
[   11.045589][  T298] send message failed!
[   11.049570][  T298] send message failed!
[   11.053569][  T298] send message failed!
[   11.057647][  T298] send message failed!
[   11.061737][  T298] send message failed!
[   11.065844][  T298] send message failed!
[   11.070288][  T298] send message failed!
[   11.074500][  T298] send message failed!
[   11.078607][  T298] send message failed!
[   11.083135][  T298] send message failed!
[   11.087286][  T298] send message failed!
[   11.091463][  T298] receive power state report with value 0
[   11.097631][  T298] send message failed!
[   11.101855][  T298] send message failed!
[   11.105864][  T298] send message failed!
[   11.109870][  T298] send message failed!
[   11.114268][  T298] send message failed!
[   11.118319][  T298] send message failed!
[   11.122381][  T298] send message failed!
[   11.126528][  T298] send message failed!
[   11.130601][  T298] send message failed!
[   11.134777][  T298] send message failed!
[   11.139090][  T298] send message failed!
[   11.143115][  T298] send message failed!
[   11.147194][  T298] send message failed!
[   11.151277][  T298] send message failed!
[   11.155363][  T298] send message failed!
[   11.159416][  T298] send message failed!
[   11.163466][  T298] send message failed!
[   11.167508][  T298] send message failed!
[   11.171556][  T298] send message failed!
[   11.175542][  T298] send message failed!
[   11.179542][  T298] send message failed!
[   11.183534][  T298] send message failed!
[   11.187527][  T298] send message failed!
[   11.191527][  T298] send message failed!
[   11.195530][  T298] send message failed!
[   11.199561][  T298] send message failed!
[   11.203594][  T298] send message failed!
[   11.207603][  T298] send message failed!
[   11.211625][  T298] send message failed!
[   11.521304][   T10] imx6q-pcie 5f000000.pcie: No cache used with register defaults set!
[   11.566654][   T10] imx6q-pcie 5f000000.pcie: PCIe PLL is locked.
[   11.573002][   T10] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[   11.579313][   T10] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[   11.587612][   T10] imx6q-pcie 5f000000.pcie: host bridge /bus@5f000000/pcie@0x5f000000 range
s:
[   11.596392][   T10] imx6q-pcie 5f000000.pcie:       IO 0x006ff80000..0x006ff8ffff -> 0x000000
0000
[   11.605299][   T10] imx6q-pcie 5f000000.pcie:      MEM 0x0060000000..0x006fefffff -> 0x006000
0000
[   11.614271][   T10] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[   11.620598][   T10] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[   12.626596][   T10] imx6q-pcie 5f000000.pcie: Phy link never came up
[   12.634177][   T10] imx6q-pcie: probe of 5f000000.pcie failed with error -110
[   12.688251][  T277] F2FS-fs (dm-10): Using encoding defined by superblock: utf8-12.1.0 with f
lags 0x0
[   12.718300][  T277] F2FS-fs (dm-10): Mounted with checkpoint version = 7a83d964
[   12.863726][  T281] type=1400 audit(1689388939.788:5): avc: denied { sys_admin } for comm="an
droid.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0
 tclass=capability permissive=0
[   12.883902][  T281] type=1400 audit(1689388939.788:6): avc: denied { sys_admin } for comm="an
droid.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0
 tclass=capability permissive=0
[   12.934845][    T1] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
[   13.087351][  T277] vold: keystore2 Keystore earlyBootEnded returned service specific error: 
-68
[   13.183246][  T274] logd: logd reinit
[   13.190651][  T274] logd: FrameworkListener: read() failed (Connection reset by peer)
[   13.191432][  T388] apexd: This device does not support updatable APEX. Exiting
[   13.205991][  T388] apexd: Marking APEXd as activated
[   13.236631][  T201] debugfs: File 'Playback' in directory 'dapm' already present!
[   13.244211][  T201] debugfs: File 'Capture' in directory 'dapm' already present!
[   13.263000][    T1] init: Not setting encryption policy on: /data/system_ce
[   13.270408][    T1] init: Not setting encryption policy on: /data/misc_de
[   13.277587][    T1] init: Not setting encryption policy on: /data/misc_ce
[   13.284789][    T1] init: Not setting encryption policy on: /data/user
[   13.291799][    T1] init: Not setting encryption policy on: /data/user_de
[   13.299593][    T1] init: Command 'rm /data/user/0' action=post-fs-data (/system/etc/init/hw/
init.rc:915) took 0ms and failed: unlink() failed: Is a directory
[   13.333149][    T1] init: Verified that /data/cache has the encryption policy bb09fc91faf1e41
246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.347340][    T1] init: Verified that /data/rollback has the encryption policy bb09fc91faf1
e41246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.360443][    T1] init: Verified that /data/rollback-observer has the encryption policy bb0
9fc91faf1e41246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.373669][    T1] init: Inferred action different from explicit one, expected 2 but got 3
[   13.434891][  T394] cs42xx8 1-0048: failed to get device ID, ret = -1
[   13.442164][  T394] cs42xx8: probe of 1-0048 failed with error -1
[   13.568915][  T399] fec 5b040000.ethernet: Adding to iommu group 2
[   13.578147][  T399] pps pps0: new PPS source ptp0
[   13.595367][  T399] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing.
[   13.607256][  T399] fec 5b040000.ethernet eth0: registered PHC device 0
[   13.718197][  T403] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   13.727146][  T403] cfg80211: Problem loading in-kernel X.509 certificate (-13)
[   13.727598][  T281] type=1400 audit(1689388940.652:7): avc: denied { write } for comm="insmod
" scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-insmod-sh:s0 tclass=key permissive=0
[   13.753221][  T155] cfg80211: loaded regulatory.db is malformed or signature is missing/inval
id
[   13.753586][  T281] type=1400 audit(1689388940.676:8): avc: denied { search } for comm="kwork
er/1:10" scontext=u:r:kernel:s0 tcontext=u:r:init-insmod-sh:s0 tclass=key permissive=0
[   13.879670][  T409] apexd: This device does not support updatable APEX. Exiting
[   13.887053][  T409] apexd: Marking APEXd as ready
[   13.916838][  T410] mlan: loading out-of-tree module taints kernel.
[   13.999929][    T1] WARNING: Unprivileged eBPF is enabled, data leaks possible via Spectre v2
 BHB attacks!
[   14.036780][  T412] wlan: Loading MWLAN driver
[   14.042104][  T412] wlan: Register to Bus Driver...
[   14.049974][  T412] wlan: Register to Bus Driver Done
[   14.055122][  T412] wlan: Driver loaded successfully
[   14.062952][  T415] LibBpfLoader: Section bpfloader_min_ver value is 2 [0x2]
[   14.070304][  T415] LibBpfLoader: Section bpfloader_max_ver value is 65536 [0x10000]
[   14.078338][  T415] LibBpfLoader: Section size_of_bpf_map_def value is 116 [0x74]
[   14.085972][  T415] LibBpfLoader: Section size_of_bpf_prog_def value is 92 [0x5c]
[   14.093550][  T415] LibBpfLoader: BpfLoader version 0x00013 processing ELF object /apex/com.a
ndroid.tethering/etc/bpf/offload.o with ver [0x00002,0x10000)
[   14.134527][  T417] remoteproc remoteproc1: imx-dsp-rproc is available
[   15.944403][  T415] printk: bpfloader: 1679 output lines suppressed due to ratelimiting
[   15.993543][  T429] update_verifier: Started with arg 1: nonencrypted
[   16.003542][  T429] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[   16.010727][  T429] update_verifier: Leaving update_verifier.
[   16.100693][  T236] Mass Storage Function, version: 2009/09/11
[   16.106618][  T236] LUN: removable file: (no medium)
[   16.116711][  T236] using random self ethernet address
[   16.121969][  T236] using random host ethernet address
[   16.128026][  T236] file system registered
[   16.383345][  T454] healthd: No battery devices found
[   16.411578][  T454] healthd: battery none chg=u
[   16.541126][  T281] type=1400 audit(1689388943.464:9): avc: denied { read } for comm="android
.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontrol
_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   16.602873][  T281] type=1400 audit(1689388943.528:10): avc: denied { integrity } for comm="i
nit" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown 
permissive=0
[   16.621508][  T281] type=1400 audit(1689388943.528:11): avc: denied { integrity } for comm="i
nit" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown 
permissive=0
[   16.847979][  T497] amphion-vpu-core 2d090000.vpu-core: encoder firmware version : 1.3.3
[   16.884900][  T497] amphion-vpu-core 2d080000.vpu-core: decoder firmware version : 1.8.6
[   17.473082][  T570] read descriptors
[   17.476768][  T570] read strings
[   18.342478][  T172] android_work: sent uevent USB_STATE=CONNECTED
[   18.351560][  T172] android_work: sent uevent USB_STATE=CONFIGURED
[   18.411905][  T272] logd: logdr: UID=1036 GID=1007 PID=566 b tail=0 logMask=bf pid=0 start=16
89388918381464000ns deadline=0ns
[   20.824179][  T281] type=1400 audit(1689388947.748:12): avc: denied { read } for comm="main" 
name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=318 scontext=u:r:zygote:s0 tcontext=u:o
bject_r:vendor_default_prop:s0 tclass=file permissive=0
[   21.575624][  T281] type=1400 audit(1689388948.500:13): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   24.598150][    T1] init: service 'idmap2d' requested start, but it is already running (flags
: 4)
[   24.607211][    T1] init: Control message: Processed ctl.start for 'idmap2d' from pid: 619 (s
ystem_server)
[   24.794386][  T454] healthd: battery none chg=u
[   25.224294][    T1] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/system/et
c/init/hw/init.rc:1193)
[   25.235860][    T1] init: starting service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)'
...
[   25.251181][    T1] init: SVC_EXEC service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)'
 pid 710 (uid 0 gid 0+0 context default) started; waiting...
[   25.650192][    T1] init: Service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)' (pid 710
) exited with status 0 waiting took 0.402000 seconds
[   25.663523][    T1] init: Sending signal 9 to service 'exec 19 (/system/bin/extra_free_kbytes
.sh 24300)' (pid 710) process group...
[   25.675956][    T1] libprocessgroup: Successfully killed process cgroup uid 0 pid 710 in 0ms
[   26.166030][  T691] read descriptors
[   26.169768][  T691] read strings
[   26.173248][  T691] read descriptors
[   26.176922][  T691] read strings
[   26.567414][  T431] Qualcomm Atheros AR8031/AR8033 5b040000.ethernet-1:00: attached PHY drive
r (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
[   26.584608][  T281] type=1400 audit(1689388953.508:14): avc: denied { read } for comm="main" 
name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=318 scontext=u:r:zygote:s0 tcontext=u:o
bject_r:vendor_default_prop:s0 tclass=file permissive=0
[   26.610659][  T281] type=1400 audit(1689388953.532:15): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   28.459475][  T281] type=1400 audit(1689388955.384:16): avc: granted { read } for comm="rksta
ck.process" name="psched" dev="proc" ino=4026531994 scontext=u:r:network_stack:s0 tcontext=u:obj
ect_r:proc_net:s0 tclass=file
[   28.482878][  T281] type=1400 audit(1689388955.404:17): avc: granted { read open } for comm="
rkstack.process" path="/proc/878/net/psched" dev="proc" ino=4026531994 scontext=u:r:network_stac
k:s0 tcontext=u:object_r:proc_net:s0 tclass=file
[   28.506009][  T281] type=1400 audit(1689388955.404:18): avc: granted { getattr } for comm="rk
stack.process" path="/proc/878/net/psched" dev="proc" ino=4026531994 scontext=u:r:network_stack:
s0 tcontext=u:object_r:proc_net:s0 tclass=file
[   28.592879][  T313] send message failed!
[   28.647104][  T313] send message failed!
[   28.660177][  T313] send message failed!
[   28.666762][  T313] receive power state report with value 0
[   28.672776][  T313] send message failed!
[   29.109733][    T1] init: processing action (boot.car_service_created=1) from (/system/etc/in
it/com.android.car.procfsinspector.rc:7)
[   29.124773][    T1] init: starting service 'com.android.car.procfsinspector'...
[   29.178070][  T313] send message failed!
[   31.686098][  T281] type=1400 audit(1689388958.608:19): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   32.012042][    T1] init: processing action (sys.boot_completed=1) from (/system/etc/init/hw/
init.rc:1184)
[   32.023583][    T1] init: starting service 'exec 21 (/bin/rm -rf /data/per_boot)'...
[   32.038386][    T1] init: SVC_EXEC service 'exec 21 (/bin/rm -rf /data/per_boot)' pid 1541 (u
id 1000 gid 1000+0 context default) started; waiting...
[   32.073214][    T1] init: Service 'exec 21 (/bin/rm -rf /data/per_boot)' (pid 1541) exited wi
th status 0 waiting took 0.036000 seconds
[   32.086741][    T1] init: Sending signal 9 to service 'exec 21 (/bin/rm -rf /data/per_boot)' 
(pid 1541) process group...
[   32.098826][    T1] libprocessgroup: Successfully killed process cgroup uid 1000 pid 1541 in 
0ms
[   32.115874][    T1] init: Encryption policy of /data/per_boot set to 96a81c4fc373aab9cf654b0d
1b75c442 v2 modes 1/4 flags 0xa
[   32.130190][    T1] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/
init.nxp.rc:199)
[   32.182408][    T1] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/
init.nxp.imx8qm.rc:48)
[   32.219000][    T1] init: processing action (sys.boot_completed=1 && vendor.all.car=true) fro
m (/vendor/etc/init/hw/init.nxp.imx8qm.rc:86)
[   32.249040][  T236] vehicle_rpmsg virtio0.rpmsg-vehicle-channel.-1.1: new channel: 0x401 -> 0
x1!
[   32.264864][  T172] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[   32.277474][  T172] debugfs: Directory 'img-pdma1' with parent 'pm_genpd' already present!
[   32.288410][  T172] debugfs: Directory 'img-pdma2' with parent 'pm_genpd' already present!
[   32.299195][  T172] debugfs: Directory 'img-pdma3' with parent 'pm_genpd' already present!
[   32.308639][  T172] debugfs: Directory 'img-pdma4' with parent 'pm_genpd' already present!
[   32.324046][  T172] debugfs: Directory 'img-pdma5' with parent 'pm_genpd' already present!
[   32.332710][  T172] debugfs: Directory 'img-pdma6' with parent 'pm_genpd' already present!
[   32.342487][  T172] debugfs: Directory 'img-pdma7' with parent 'pm_genpd' already present!
[   32.409980][  T172] imx-lpi2c 57247000.i2c: use pio mode
[   32.416717][  T172] i2c 5-004c: Fixing up cyclic dependency with bus@57240000:ldb@572410e0
[   33.434963][  T172] it6263 5-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[   33.443357][  T172] i2c i2c-5: LPI2C adapter registered
[   33.631745][  T172] platform 57180000.dpu: Fixing up cyclic dependency with 57228000.dsi_host
[   33.646186][  T172] dpu-core 57180000.dpu: driver probed
[   33.648094][  T176] ***************************bfz panel probe in****************************
****
[   33.663385][  T176] panel-raydium-rm67191 57228000.dsi_host.0: nonexclusive access to GPIO fo
r reset
[   33.672966][  T176] panel-raydium-rm67191 57228000.dsi_host.0: supply v3p3 not found, using d
ummy regulator
[   33.683382][  T176] panel-raydium-rm67191 57228000.dsi_host.0: supply v1p8 not found, using d
ummy regulator
[   33.694077][  T176] nwl-dsi 57228000.dsi_host: [drm:nwl_dsi_host_attach [nwl_dsi]] lanes=4, f
ormat=0x0 flags=0x215
[   33.704847][  T176] ******************bfz panel probe out*******************
[   33.720512][  T172] imx-lpi2c 58226000.i2c: use pio mode
[   33.722774][  T176] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_o
ps)
[   33.732080][  T172] i2c i2c-6: LPI2C adapter registered
[   33.759307][  T176] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_o
ps)
[   33.763631][  T172] imx-lpi2c 58246000.i2c: use pio mode
[   33.778712][  T172] i2c i2c-7: LPI2C adapter registered
[   33.785635][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[   33.787776][  T172] mxc-md bus@58000000:camera: deferring cap_device registration
[   33.800816][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[   33.806048][  T172] isi-capture 58100000.isi:cap_device: deferring 58100000.isi:cap_device de
vice registration
[   33.815564][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[   33.822275][  T172] isi-m2m 58100000.isi:m2m_device: deferring 58100000.isi:m2m_device device
 registration
[   33.839672][  T172] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[   33.847599][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[   33.849134][  T172] isi-capture 58110000.isi:cap_device: deferring 58110000.isi:cap_device de
vice registration
[   33.866133][  T176] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component
_ops [nwl_dsi])
[   33.877255][  T172] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[   33.878484][  T176] imx-drm display-subsystem: bound bus@56240000:ldb@562410e0 (ops imx8qm_ld
b_ops [imx8qm_ldb])
[   33.910021][  T172] isi-capture 58120000.isi:cap_device: deferring 58120000.isi:cap_device de
vice registration
[   33.920573][  T176] imx-drm display-subsystem: bound 57228000.dsi_host (ops nwl_dsi_component
_ops [nwl_dsi])
[   33.931166][  T172] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[   33.938971][  T176] imx-drm display-subsystem: bound bus@57240000:ldb@572410e0 (ops imx8qm_ld
b_ops [imx8qm_ldb])
[   33.947884][  T172] isi-capture 58130000.isi:cap_device: deferring 58130000.isi:cap_device de
vice registration
[   33.960103][  T176] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[   33.964036][  T172] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[   33.977996][  T182] vref_1v8: disabling
[   33.982066][  T182] SD3_SPWR: disabling
[   33.983082][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   33.987150][  T172] isi-capture 58140000.isi:cap_device: deferring 58140000.isi:cap_device de
vice registration
[   33.999702][  T176] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[   34.004170][  T172] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[   34.021500][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   34.021852][  T172] isi-capture 58150000.isi:cap_device: deferring 58150000.isi:cap_device de
vice registration
[   34.029823][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   34.039017][  T172] mxc-isi 58150000.isi: mxc_isi.5 registered successfully
[   34.046786][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   34.055112][  T172] isi-capture 58160000.isi:cap_device: deferring 58160000.isi:cap_device de
vice registration
[   34.061178][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video6
[   34.070442][  T172] mxc-isi 58160000.isi: mxc_isi.6 registered successfully
[   34.077559][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   34.086727][  T172] isi-capture 58170000.isi:cap_device: deferring 58170000.isi:cap_device de
vice registration
[   34.102526][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   34.103175][  T172] mxc-isi 58170000.isi: mxc_isi.7 registered successfully
[   34.110598][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   34.124447][  T172] platform 58227000.csi: Fixing up cyclic dependency with 6-006a
[   34.127573][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   34.139316][  T496] audit: audit_lost=1 audit_rate_limit=5 audit_backlog_limit=64
[   34.139461][  T281] type=1400 audit(1689388961.064:20): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.141010][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video6
[   34.141640][  T176] mx8-img-md: Registered mxc_isi.4.capture as /dev/video7
[   34.142079][  T176] mx8-img-md: Registered mxc_isi.5.capture as /dev/video8
[   34.142468][  T176] mx8-img-md: Registered mxc_isi.6.capture as /dev/video9
[   34.142705][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   34.146950][  T496] audit: rate limit exceeded
[   34.154797][  T172] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[   34.169902][  T176] max9286_mipi 6-006a: max9286_read_reg:read reg error: reg=1e
[   34.171461][  T281] type=1400 audit(1689388961.064:21): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173321][  T281] type=1400 audit(1689388961.064:22): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173466][  T281] type=1400 audit(1689388961.064:23): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173564][  T281] type=1400 audit(1689388961.064:24): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173660][  T281] type=1400 audit(1689388961.064:25): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173755][  T281] type=1400 audit(1689388961.064:26): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173866][  T281] type=1400 audit(1689388961.064:27): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173962][  T281] type=1400 audit(1689388961.064:28): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.180179][  T172] platform 58247000.csi: Fixing up cyclic dependency with 7-006a
[   34.184169][  T176] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[   34.271942][  T172] mxc-mipi-csi2 58247000.csi: lanes: 4, name: mxc-mipi-csi2.1
[   34.361424][  T176] max9286_mipi 7-006a: max9286_read_reg:read reg error: reg=1e
[   34.392585][  T172] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video3 (81,3
)
[   34.406777][  T176] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[   34.417690][  T172] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video4 (81,4
)
[   34.423138][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video5
[   34.469391][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video6
[   34.477536][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video7
[   34.516172][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video8
[   34.524003][  T176] mx8-img-md: Registered mxc_isi.4.capture as /dev/video9
[   34.531574][  T176] mx8-img-md: Registered mxc_isi.5.capture as /dev/video10
[   34.563754][  T176] mx8-img-md: Registered mxc_isi.6.capture as /dev/video11
[   34.571512][  T176] mx8-img-md: Registered mxc_isi.7.capture as /dev/video12
[   34.580859][  T176] unregister ISI channel: mxc_isi.0
[   34.586795][  T176] unregister ISI channel: mxc_isi.1
[   34.592453][  T176] unregister ISI channel: mxc_isi.2
[   34.598333][  T176] unregister ISI channel: mxc_isi.3
[   34.604250][  T176] unregister ISI channel: mxc_isi.4
[   34.614715][  T176] unregister ISI channel: mxc_isi.5
[   34.621148][  T176] unregister ISI channel: mxc_isi.6
[   34.627237][  T176] unregister ISI channel: mxc_isi.7
[   34.947670][  T496] ***************************bfz panel init in*****************************
***
[   34.996076][ T1730] ci_hdrc ci_hdrc.0: EHCI Host Controller
[   35.001736][ T1730] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[   35.022647][ T1730] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[   35.026609][  T496] ***************************bfz panel init out****************************
****
[   35.029089][ T1730] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice=
 5.15
[   35.046751][ T1730] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   35.055284][ T1730] usb usb1: Product: EHCI Host Controller
[   35.060927][ T1730] usb usb1: Manufacturer: Linux 5.15.71-g279b46e22312-dirty ehci_hcd
[   35.068879][ T1730] usb usb1: SerialNumber: ci_hdrc.0
[   35.074644][ T1730] hub 1-0:1.0: USB hub found
[   35.079185][ T1730] hub 1-0:1.0: 1 port detected
[   35.100542][ T1730] insmod (1730) used greatest stack depth: 9600 bytes left
[   35.607695][  T496] ***************************bfz panel init in*****************************
***
[   35.686601][  T496] ***************************bfz panel init out****************************
****
[   36.756565][  T281] type=1400 audit(1689388963.680:61): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   38.547308][  T644] binder_alloc: 2009: binder_alloc_buf, no vma
[   38.555262][  T644] binder: 619:644 transaction failed 29189/-3, size 3564-8 line 3101
[   40.961761][    T1] init: Sending signal 9 to service 'idmap2d' (pid 533) process group...
[   40.981303][    T1] libprocessgroup: Successfully killed process cgroup uid 1000 pid 533 in 1
1ms
[   40.994891][    T1] init: Control message: Processed ctl.stop for 'idmap2d' from pid: 619 (sy
stem_server)
[   41.004826][  T643] binder_alloc: 2394: binder_alloc_buf, no vma
[   41.005509][    T1] init: Service 'idmap2d' (pid 533) received signal 9
[   41.011670][  T643] binder: 619:643 transaction failed 29189/-3, size 88-0 line 3101
[   45.862907][  T619] binder_alloc: 3159: binder_alloc_buf, no vma
[   45.879346][  T619] binder: 619:619 transaction failed 29189/-3, size 136-0 line 3101
[   56.382579][    C2] Unable to handle kernel paging request at virtual address dead00000000012
a
[   56.382643][   T20] Kernel panic - not syncing: CFI failure (target: rad_panel_probe.9c599efe
498b8cff52ce0fab43b5b106.cfi_jt+0x0/0x4)
[   56.391242][    C2] Mem abort info:
[   56.403250][   T20] SMP: stopping secondary CPUs
[   56.411363][    C2]   ESR = 0x96000044
[   56.415115][    C2]   EC = 0x25: DABT (current EL), IL = 32 bits
[   56.421127][    C2]   SET = 0, FnV = 0
[   56.424879][    C2]   EA = 0, S1PTW = 0
[   56.428720][    C2]   FSC = 0x04: level 0 translation fault
[   56.434297][    C2] Data abort info:
[   56.437876][    C2]   ISV = 0, ISS = 0x00000044
[   56.442411][    C2]   CM = 0, WnR = 1
[   56.446077][    C2] [dead00000000012a] address between user and kernel address ranges
[   56.453916][    C2] Internal error: Oops: 96000044 [#1] PREEMPT SMP
[   56.460199][    C2] Modules linked in: ci_hdrc_imx(E) usbmisc_imx(E) ci_hdrc(E) ulpi(E) snd_s
of_imx8(E) imx_common(E) snd_sof_xtensa_dsp(E) snd_sof_of(E) snd_sof(E) imx_dsp_rproc(E) moal(OE
) mlan(OE) mac80211(E) cfg80211(E) fec(E) at803x(E) snd_soc_cs42xx8_i2c(E) snd_soc_cs42xx8(E) sn
d_soc_fsl_esai(E) snd_soc_bt_sco(E) spi_slave_system_control(E) spi_slave_time(E) spi_imx(E) spi
_fsl_lpspi(E) spi_bitbang(E) spidev(E) pci_imx6(E) phy_fsl_imx8_pcie(E) snd_soc_fsl_sai(E) imx_p
cm_dma(E) snd_soc_fsl_asoc_card(E) snd_soc_imx_audmux(E) snd_soc_simple_card(E) snd_soc_simple_c
ard_utils(E) snd_soc_wm8960(E) mx3fb(E) fb_fence(E) mxc_edid(E) cfbimgblt(E) cfbcopyarea(E) cfbf
illrect(E) fb(E) fb_notify(E) imx_sc_thermal(E) galcore(E) device_cooling(E) vehicle_rpmsg_m4(E)
 mux_mmio(E) trusty_virtio(E) trusty_ipc(E) trusty_log(E) trusty_irq(E) vehicle_core(E) imx_rpro
c(E) imx8_parallel_csi(CE) imx8_media_dev(CE) gmsl_max9286(CE) imx8_capture(CE) imx8_isi_capture
(CE) imx8_isi_mem2mem(CE)
[   56.460492][    C2]  imx8_isi_hw(CE) dwc_mipi_csi2(CE) imx8_mipi_csi2_sam(CE) imx8_mipi_csi2(
CE) timer_imx_sysctr(E) seco_mu(E) imx_dsp(E) sdhci_esdhc_imx(E) cqhci(E) imx_cpufreq_dt(E) cpuf
req_dt(E) imx_sc_wdt(E) amphion_vpu(E) mxc_mipi_csi2_yav(E) mxc_jpeg_encdec(E) v4l2_jpeg(E) ov56
40(E) v4l2_fwnode(E) v4l2_async(E) rtc_imx_sc(E) imx_sc_pwrkey(E) cdns3_imx(E) cdns3(E) cdns_usb
_common(E) gpio_switch(E) phy_mxs_usb(E) i2c_dev(E) i2c_mux_pca954x(E) i2c_mux(E) i2c_rpmsg_imx(
E) i2c_imx_lpi2c(E) dma_buf_imx(E) secure_heap(E) dsp_heap(E) cma_heap(E) system_heap(E) it6263(
E) nwl_dsi(E) mux_core(E) adv7511(E) cdns_mhdp_imx(E) cdns_mhdp_drmcore(E) imx_dcss(E) sec_mipi_
dsim_imx(E) sec_dsim(E) imx8qxp_ldb(E) imx8qm_ldb(E) fsl_imx_ldb(E) imx_ldb(E) arm_smmu_v3(E) ar
m_smmu(E) qcom_scm(E) fsl_lpuart(E) pf8x00_regulator(E) gpio_regulator(E) imx8m_pm_domains(E) bu
sfreq_imx8mq(E) mxs_dma(E) stmp_device(E) fsl_edma_v3(E) pwm_bl(E) pwm_imx27(E) nvmem_imx_ocotp_
scu(E) gpio_pca953x(E)
[   56.546562][    C2]  pinctrl_imx8qxp(E) pinctrl_imx8qm(E) pinctrl_scu(E) pinctrl_imx(E) phy_m
ixel_lvds_combo(E) phy_mixel_lvds(E) phy_fsl_samsung_hdmi(E) phy_fsl_imx8_mipi_dphy(E) phy_caden
ce_salvo(E) irq_imx_irqsteer(E) trusty_core(E) zsmalloc(E)
[   56.654032][    C2] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G         C OE     5.15.71-g279b46
e22312-dirty #14
[   56.663960][    C2] Hardware name: Freescale i.MX8QM MEK (DT)
[   56.669712][    C2] pstate: 804000c5 (Nzcv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   56.677382][    C2] pc : expire_timers+0xa8/0x1a0
[   56.682108][    C2] lr : __run_timers+0x180/0x1e4
[   56.686825][    C2] sp : ffffffc00a94bdf0
[   56.690839][    C2] x29: ffffffc00a94be00 x28: ffffffc00a853260 x27: ffffff8810303600
[   56.698692][    C2] x26: ffffffc00a66adf8 x25: ffffffc00a63d008 x24: dead000000000122
[   56.706546][    C2] x23: 0000000000000000 x22: ffffffc00a90d278 x21: 00000000ffff1200
[   56.714399][    C2] x20: ffffff88fcf6ef80 x19: ffffffc00a94be60 x18: ffffffc00a941038
[   56.722252][    C2] x17: ffffffc8f292f000 x16: 0000000000000000 x15: 0000000000000000
[   56.730106][    C2] x14: ffffffc00a90d278 x13: ffffff88fcf6f638 x12: 0000000000000040
[   56.737960][    C2] x11: ffffffc00a94be68 x10: ffffffffffffffff x9 : ffffffc00a94be60
[   56.745813][    C2] x8 : dead000000000122 x7 : 0000000000000001 x6 : fffffffdefb88a90
[   56.753667][    C2] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000200
[   56.761520][    C2] x2 : 0000000000000200 x1 : ffffffc00a94be60 x0 : ffffff88fcf6ef80
[   56.769384][    C2] Call trace:
[   56.772530][    C2]  expire_timers+0xa8/0x1a0
[   56.776897][    C2]  __run_timers+0x180/0x1e4
[   56.781267][    C2]  run_timer_softirq+0x28/0x58
[   56.785897][    C2]  _stext+0x134/0x4bc
[   56.789746][    C2]  __irq_exit_rcu.llvm.16159328691032069789+0x74/0x100
[   56.796461][    C2]  handle_domain_irq+0x80/0xf4
[   56.801092][    C2]  gic_handle_irq+0x54/0x114
[   56.805548][    C2]  call_on_irq_stack+0x3c/0x6c
[   56.810179][    C2]  do_interrupt_handler+0x44/0xa0
[   56.815070][    C2]  el1_interrupt+0x34/0x64
[   56.819353][    C2]  el1h_64_irq_handler+0x1c/0x2c
[   56.824157][    C2]  el1h_64_irq+0x7c/0x80
[   56.828266][    C2]  arch_local_irq_enable+0xc/0x18
[   56.833157][    C2]  default_idle_call+0x40/0x150
[   56.837875][    C2]  do_idle.llvm.13579087976232309098+0x100/0x2b8
[   56.844069][    C2]  cpu_startup_entry+0x28/0x2c
[   56.848699][    C2]  secondary_start_kernel+0x1ac/0x214
[   56.853938][    C2]  __secondary_switched+0x94/0x98
[   56.858836][    C2] Code: d503201f a94026c8 f9000128 b4000048 (f9000509) 
[   56.865633][    C2] ---[ end trace e36c04e90a71d350 ]---
[   56.894395][   T20] Kernel Offset: disabled
[   56.898583][   T20] CPU features: 0x2,00004163,20000846
[   56.903813][   T20] Memory Limit: none
[   56.907573][   T20] trusty-log trusty:trusty-log: panic notifier - trusty version Project: im
x8qm_a72, Build: build@pantakill-5, Built: 10:05:29 Nov  8 2022

U-Boot SPL 2022.04-g93f803c3-dirty (Jul 17 2023 - 09:15:59 +0800)
Normal Boot
Trying to boot from MMC1
Authentication key not yet programmed 
Booting from bootloader_a...
UU
  boot args 0x*** 0x*** 0x*** 0x0
initializing trusty (Project: imx8qm_a72, Build: build@pantakill-5, Built: 10:05:29 Nov  8 2022)
Core:  180 devices, 28 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0i2c: Error check busy bus: 0x8
it6263_i2c_reg_read, read err -102
faill to read from it6263 revision, ret -102
 (1280 x 720)
        [0] dpu@56180000, video
        [1] lvds-channel@0, display
        [2] lvds-to-hdmi-bridge@4c, video_bridge
In:    serial
Out:   serial
Err:   serial

 BuildInfo: 
  - SCFW 6638c032, SECO-FW c9de51c0, IMX-MKIMAGE d265bd1e, ATF 503f7fe
  - U-Boot 2022.04-g93f803c3-dirty 

flash target is MMC:0
Net:   eth0: ethernet@5b040000 [PRIME], eth1: ethernet@5b050000
INFO Initializing Trusty device
INFO selected trusty api version: 3 (requested 3)
INFO Initializing Trusty IPC device
INFO Initializing RPMB storage proxy service
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
failed to read rpmb write counter
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
ss: block_device_tipc_init: bad static rpmb size, 2048
ss: proxy_connect: block_device_tipc_init failed (-1)
Authentication key not yet programmed 
INFO Initializing Trusty Hardware Crypto client
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
Verifying slot _a ...
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_validate_vbmeta_public_key_rpmb: Read public key error
avb_slot_verify.c:899: ERROR: vbmeta_a: Public key used to sign data rejected.
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
 verify FAIL, state: UNLOCK
 boot 'boot_a' still
Kernel load addr 0x80280000 size 21813 KiB
kernel   @ 80280000 (43253760)
ramdisk  @ fc000000 (19757977)
fdt      @ 82d40400 (138738)
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
ERROR - failed to read public key for keymaster
keymaster.c:318: ERROR Keymaster TIPC client not initialized!
keymaster.c:684: ERROR Keymaster TIPC client not initialized!
boota: set boot patch level failed.
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
Authentication key not yet programmed 
Moving Image from 0x80280000 to 0x80400000, end=82d40000
## Flattened Device Tree blob at 82d40400
   Booting using the fdt blob at 0x82d40400
ERROR: reserving fdt memory region failed (addr=900ff000 size=1000 flags=4)
ERROR: reserving fdt memory region failed (addr=90400000 size=100000 flags=4)
ERROR: reserving fdt memory region failed (addr=90100000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90108000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90110000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90118000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=901ff000 size=1000 flags=4)
ERROR: reserving fdt memory region failed (addr=91f00000 size=100000 flags=0)
   Using Device Tree in place at 0000000082d40400, end 0000000082d651f1

Starting kernel ...

[    0.000000][    T0] Booting Linux on physical CPU 0x0000000100 [0x410fd082]
[    0.000000][    T0] Linux version 5.15.71-g279b46e22312-dirty (bfz@bfz) (Android (8508608, ba
sed on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4
c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #14 SMP PREEMPT Mon Jul 17 09:33:11 CST 20
23
[    0.000000][    T0] Machine model: Freescale i.MX8QM MEK
[    0.000000][    T0] Stack Depot is disabled
[    0.000000][    T0] earlycon: lpuart32 at MMIO32 0x000000005a060000 (options '')
[    0.000000][    T0] printk: bootconsole [lpuart32] enabled
[    0.000000][    T0] efi: UEFI not found.
[    0.000000][    T0] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 Mi
B
[    0.000000][    T0] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-p
ool
[    0.000000][    T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 Mi
B
[    0.000000][    T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id sh
ared-dma-pool
[    0.000000][    T0] kvm [0]: Reserved 36 MiB at 0x97d000000
[    0.000000][    T0] Zone ranges:
[    0.000000][    T0]   DMA32    [mem 0x0000000080200000-0x00000000ffffffff]
[    0.000000][    T0]   Normal   [mem 0x0000000100000000-0x000000097fffffff]
[    0.000000][    T0] Movable zone start for each node
[    0.000000][    T0] Early memory node ranges
[    0.000000][    T0]   node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000084000000-0x00000000863fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000086400000-0x00000000887fffff]
[    0.000000][    T0]   node   0: [mem 0x000000008a800000-0x000000008fffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000090c00000-0x0000000091ffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092000000-0x00000000920fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092100000-0x00000000923fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092400000-0x00000000951fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000095200000-0x00000000fdffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000880000000-0x000000088fffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000890000000-0x000000097fffffff]
[    0.000000][    T0] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff]
[    0.000000][    T0] On node 0, zone DMA32: 512 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone DMA32: 8192 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone DMA32: 3072 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone Normal: 8192 pages in unavailable ranges
[    0.000000][    T0] cma: Reserved 928 MiB at 0x00000000c2000000
[    0.000000][    T0] psci: probing for conduit method from DT.
[    0.000000][    T0] psci: PSCIv1.1 detected in firmware.
[    0.000000][    T0] psci: Using standard PSCI v0.2 function IDs
[    0.000000][    T0] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000][    T0] psci: SMC Calling Convention v1.2
[    0.000000][    T0] Load bootconfig: 1018 bytes 64 nodes
[    0.000000][    T0] percpu: Embedded 29 pages/cpu s81752 r8192 d28840 u118784
[    0.000000][    T0] Detected PIPT I-cache on CPU0
[    0.000000][    T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[    0.000000][    T0] CPU features: detected: GIC system register CPU interface
[    0.000000][    T0] CPU features: detected: Spectre-v2
[    0.000000][    T0] CPU features: detected: Spectre-v3a
[    0.000000][    T0] CPU features: detected: Spectre-BHB
[    0.000000][    T0] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000][    T0] Built 1 zonelists, mobility grouping on.  Total pages: 1528328
[    0.000000][    T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.
mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init firmware_class.
path=/vendor/firmware loop.max_part=7 bootconfig cma=928M@0x960M-0xfc0M transparent_hugepage=nev
er moal.mod_para=wifi_mod_para.conf pci=nomsi video=HDMI-A-2:d bootconfig buildvariant=userdebug
[    0.000000][    T0] cgroup: Disabling pressure control group feature
[    0.000000][    T0] Unknown kernel command line parameters "buildvariant=userdebug", will be 
passed to user space.
[    0.000000][    T0] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linea
r)
[    0.000000][    T0] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000][    T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[    0.000000][    T0] software IO TLB: mapped [mem 0x00000000be000000-0x00000000c2000000] (64MB
)
[    0.000000][    T0] Memory: 4624248K/6211584K available (18496K kernel code, 2262K rwdata, 19
172K rodata, 1472K init, 613K bss, 637064K reserved, 950272K cma-reserved)
[    0.000000][    T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1
[    0.000000][    T0] trace event string verifier disabled
[    0.000000][    T0] rcu: Preemptible hierarchical RCU implementation.
[    0.000000][    T0] rcu:     RCU event tracing is enabled.
[    0.000000][    T0] rcu:     RCU dyntick-idle grace-period acceleration is enabled.
[    0.000000][    T0] rcu:     RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=6.
[    0.000000][    T0] rcu:     RCU priority boosting: priority 1 delay 500 ms.
[    0.000000][    T0]  Trampoline variant of Tasks RCU enabled.
[    0.000000][    T0]  Tracing variant of Tasks RCU enabled.
[    0.000000][    T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000][    T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6
[    0.000000][    T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000][    T0] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000][    T0] GICv3: 512 SPIs implemented
[    0.000000][    T0] GICv3: 0 Extended SPIs implemented
[    0.000000][    T0] GICv3: Distributor has no Range Selector support
[    0.000000][    T0] Root IRQ handler: gic_handle_irq.0063cfc43c850c778600e9fd9282e821.cfi_jt
[    0.000000][    T0] GICv3: 16 PPIs implemented
[    0.000000][    T0] GICv3: CPU0: found redistributor 100 region 0:0x0000000051b80000
[    0.000000][    T0] ITS: No ITS available, not enabling LPIs
[    0.000000][    T0] rcu:     Offload RCU callbacks from CPUs: (none).
[    0.000000][    T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval_
___)-0x(____ptrval____)
[    0.000000][    T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000][    T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854
df40, max_idle_ns: 440795202120 ns
[    0.000000][    T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500
ns
[    0.009339][    T0] Calibrating delay loop (skipped), value calculated using timer frequency.
. 16.00 BogoMIPS (lpj=32000)
[    0.019957][    T0] pid_max: default: 32768 minimum: 301
[    0.025423][    T0] LSM: Security Framework initializing
[    0.030603][    T0] SELinux:  Initializing.
[    0.034950][    T0] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.043020][    T0] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linea
r)
[    0.053435][    T1] rcu: Hierarchical SRCU implementation.
[    0.059252][    T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build
[    0.067755][    T1] EFI services will not be available.
[    0.073102][    T1] smp: Bringing up secondary CPUs ...
[    0.079238][    T0] Detected PIPT I-cache on CPU1
[    0.079273][    T0] GICv3: CPU1: found redistributor 101 region 0:0x0000000051ba0000
[    0.079307][    T0] CPU1: Booted secondary processor 0x0000000101 [0x410fd082]
[    0.081640][    T0] CPU features: detected: ARM erratum 845719
[    0.081659][    T0] Detected VIPT I-cache on CPU2
[    0.081694][    T0] GICv3: CPU2: found redistributor 0 region 0:0x0000000051b00000
[    0.081747][    T0] CPU2: Booted secondary processor 0x0000000000 [0x410fd034]
[   21.104265][    C0] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[   21.155629][    C0] rcu:     2-O...: (0 ticks this GP) idle=001/1/0x4000000000000004 softirq=
0/0 fqs=2625 last_accelerate: 0000/ef98 dyntick_enabled: 0
[   21.168916][    C0]  (detected by 0, t=5252 jiffies, g=-1195, q=2)
[   21.175084][    C0] rcu: Offline CPU 2 blocking current GP.
[   84.243587][    C0] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[   84.250027][    C0] rcu:     2-O...: (0 ticks this GP) idle=001/1/0x4000000000000004 softirq=
0/0 fqs=10503 last_accelerate: 0000/2d23 dyntick_enabled: 0
[   84.263405][    C0]  (detected by 0, t=21007 jiffies, g=-1195, q=2)
[   84.269659][    C0] rcu: Offline CPU 2 blocking current GP.
This is my boot log
0 件の賞賛
返信
1 返信

2,163件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using? Which version of BSP are you using? Please double check the dtb file that you are loading in the u-boot. 

0 件の賞賛
返信