i.MX8MQ-EVK: enable distro_bootcmd in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MQ-EVK: enable distro_bootcmd in u-boot

1,747件の閲覧回数
vipulkumar
Contributor III

I wanted to enable distro_bootcmd in u-boot for imx8mq-evk board.

As per this link https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/README.distro?h=imx_v2019.04_4.19.35_1...

I have made changes in u-boot.

Now I need to set following some environment variable:

1. fdt_addr and fdt_addr_r

2. ramdisk_addr_r

3. kernel_addr_r

4. pxefile_addr_r

5. scriptaddr

Where can i get memory adresses of these variables for imx8mq-evk ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,737件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

have you download or build uboot for imx8mq, if yes, when you boot up the board, you can find them in the uboot command, when the board boot up, enter any key, and use the "printenv" to check the current uboot environment

 

 

0 件の賞賛
返信

1,729件の閲覧回数
vipulkumar
Contributor III

Thanks for your reply.

I am building core-image-minimal for imx8mq-evk using instructions mentioned here:

https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-warrior

I will check.

Is imx8mq-evk supports distro_bootcmd by default ?

0 件の賞賛
返信

1,709件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

default is bootcmd, you can download prebuilt uboot to the board, after board boot up, press any key to stop it, and use "printenv" to check the uboot environment

0 件の賞賛
返信