i.MX8MP PCIe Compliance Test Enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MP PCIe Compliance Test Enable

Jump to solution
826 Views
cccku
Contributor II

Hi Community,

I am working on a custom board of i.MX8MP processor with Linux 6.1.22, and am trying to test the eye diagram of PCIe. As I am following the instructions from https://www.nxp.com/docs/en/application-note/AN12444.pdf , there is no CONFIG_PCI_IMX8_COMPLIANCE_TEST=y within the config files. I have read and referenced to case:1352394 which mentioned about IMX6_COMPLIANCE_TEST, still not found in the configs. 

Is there a workaround for such case that I could reference to?

Thank you.

Will

IMX8MPLUS

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
790 Views
joanxie
NXP TechSupport
NXP TechSupport
3 Replies
791 Views
joanxie
NXP TechSupport
NXP TechSupport

the latest bsp removed this config, pls refer to the link as below

https://github.com/nxp-imx/linux-imx/commit/05ed65b36be4b74afdf1850059139987fad956c5

785 Views
cccku
Contributor II
Hi joanxie,

Thank you for the reply.
Just for confirmation, I would only need to add the "pcie_cz_enabled=yes" in u-boot to enable the mode, is that correct?

Will
0 Kudos
Reply
781 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, correct

Tags (2)
0 Kudos
Reply