[i.MX8MP] How to generate xserver-xorg package for Yocto LF_v5.10_1.0.0 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX8MP] How to generate xserver-xorg package for Yocto LF_v5.10_1.0.0 BSP

1,596 Views
alex_cheng611
Contributor I

When I use Yocto L5.4.3_2.0.0 BSP, it can generate the xserver-xorg package for i.MX8MP with the following command:

EULA=1 DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b imx8mpevk_imx-image-full
bitbake imx-image-full

Build xserver-xorg directory:
../imx8mpevk_imx-image-full/tmp/work/aarch64-mx8mp-poky-linux/xserver-xorg

When I use Yocto LF_v5.10_1.0.0 BSP, it cannot build the xserver-xorg package with the above command.

Can you tell me how to use Yocto LF_v5.10_1.0.0 BSP to generate xserver-xorg package for i.MX8MP?

Thank you.

Labels (1)
0 Kudos
Reply
0 Replies