Hello
I want to do secure boot(HABv4) on i.MX8MP EVK using Yocto Project.
I referred to the following link.
https://github.com/nxp-imx/uboot-imx/blob/lf_v2025.04/doc/imx/habv4/guides/mx8m_secure_boot.txt
I have not burned the fuse table yet.
After boot the u-boot and run the `hab_status` command, the following events will be displayed.
u-boot=> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x40 0x1f 0xbd 0xc0
0x00 0x00 0x00 0x20STS = HAB_FAILURE (0x33)RSN = HAB_INV_ASSERTION (0x0C)CTX = HAB_CTX_ASSERT (0xA0)ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0
0x00 0x00 0x00 0x04STS = HAB_FAILURE (0x33)RSN = HAB_INV_ASSERTION (0x0C)CTX = HAB_CTX_ASSERT (0xA0)ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x34 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0b 0x48 0x40 0x1f 0xad 0xc0
0x00 0x00 0x10 0x20 0x40 0x20 0x00 0x00
0x00 0x11 0x43 0x90 0x40 0x31 0x43 0x90
0x00 0x00 0xea 0x98 0x00 0x97 0x00 0x00
0x00 0x00 0xbb 0x80 0x56 0x00 0x00 0x00
0x00 0x08 0xc3 0x80STS = HAB_FAILURE (0x33)RSN = HAB_INV_SIGNATURE (0x18)CTX = HAB_CTX_COMMAND (0xC0)ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x34 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0b 0x48 0x40 0x1f 0xad 0xc0
0x00 0x00 0x10 0x20 0x40 0x20 0x00 0x00
0x00 0x11 0x43 0x90 0x40 0x31 0x43 0x90
0x00 0x00 0xea 0x98 0x00 0x97 0x00 0x00
0x00 0x00 0xbb 0x80 0x56 0x00 0x00 0x00
0x00 0x08 0xc3 0x80STS = HAB_FAILURE (0x33)RSN = HAB_INV_SIGNATURE (0x18)CTX = HAB_CTX_COMMAND (0xC0)ENG = HAB_ENG_ANY (0x00)Questions:
1) Is it expected/normal to see these HAB events (HAB_INV_ASSERTION / HAB_INV_SIGNATURE) when fuses are not programmed yet?
2) After programming the SRK hash, should these events disappear?
Or do these events indicate that something is already wrong in my signed images/CSF/FIT setup?
thank you