i.MX8MM Accessing Board Serial Number, Assembly and Part Number in Linux OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM Accessing Board Serial Number, Assembly and Part Number in Linux OS

1,241件の閲覧回数
harsh1621
Contributor II

I've got an i.MX8MM som running Debian Buster OS and Kernel 4.19.35. I would like to access the Board Serial Number, Assembly and Part Numbers, that are displayed by the U-Boot logs, from the Linux OS.

The U-boot code seems to read these values from an on board EEPROM, is there a way to access the same from the userspace and read the values in the EEPROM?

タグ(2)
0 件の賞賛
返信
0 返答(返信)