i.MX8M Plus + UFS flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Plus + UFS flash

5,194件の閲覧回数
dav1
Contributor V

Hi NXP,

In need of large flash with high performance (256GByte+)

Curious why the i.MX8M Plus doesn't come with a UFS peripheral, seems Kioxia is pushing for this technology over traditional eMMC's

 

I know some phones use PCIe NAND flash as an alternative. Not sure what is supported in HW there on the Plus, please advice.

 

Thanks David

ラベル(1)
2 返答(返信)

5,185件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX8MPlus processor doesn't have support for UFS interface. It has the SD Host Controller module that can support regular SD and eMMC devices, and GPMI module that supports generic parallel NAND Flash. Also, it has the PCIe interface, so, PCIe mass storage devices can also be supported.

Best Regards,
Artur

0 件の賞賛
返信

4,356件の閲覧回数
dav1
Contributor V

any chance to get UFS on i.MX9 series

emmc speeds start to feel a bit vintage

0 件の賞賛
返信