i.MX8M Mini VPU and GPU Underclocking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini VPU and GPU Underclocking

1,398件の閲覧回数
adamford
Contributor II

I have an i.MX8M Mini where the the votlages for the VDD_VPU, VDD_GPU and VDD_DRAM are all tied together and operating at .95V so the LPDDR can run at 1.5GHz.

 

We're trying to lower power consumption by lowering the clocks of the VPU_H1 encoder and GPU which are both being used, but the datasheet for the i.MX8M Mini seems to show a voltage of 0.95V requires the GPU to run at 1000MHz and is too high to run the GPU at 800MHz.  The VPU_H1 seems to indicate we can run the VPU_H1 at 650MHz, but the VPU_PLL looks like it can go all the way down to 400MHz.

Can we safely underclock the VPU_H1 and 3D GPU to lower values without having to lower the DDR voltage of 0.95?

 

thank you,

Adam Ford,

Principal Applications Engineer, Beacon EmbeddedWorks.

1 返信

1,330件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @adamford, 

Based on the Reference Manual for the iMX8M Mini the GPU clock for that voltage is up to 1000MHz therefore, you might underclock this block.

Brian_Ibarra_0-1692401176307.png

However, for VPU the target frequency for H1 acceleration is 800MHz. For this case, a lower clock might generate low performance.

Brian_Ibarra_1-1692401183949.png

Best regards, Brian.

0 件の賞賛
返信