i.MX8M Mini Storage Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini Storage Temperature

1,912 Views
rfguy1
Contributor I

The temperature spec for storage for the i.MX8M Mini is -40C to 150C.  Can the processor be stored (without power) at lower temps without damage?  I wasn't sure if the -40C is specified because:

-It is related with the industrial operating temp range (-40/85C) and the measurement wasn't required or made any lower  OR

-Something within the package could be damaged if taken that low even in storage (without power).

0 Kudos
Reply
2 Replies

1,898 Views
Yuri
NXP Employee
NXP Employee

@rfguy1 
Hello,

   You are right - the storage temperature must not be lower, than -40 C, since
"something within the package could be damaged if taken that low even in storage (without power)."

Regards,
Yuri.

0 Kudos
Reply

1,910 Views
rfguy1
Contributor I

Failed to mention the interest is to -55C.

0 Kudos
Reply