i. MX8M Mini MIPI-DSI Issue Send DCS Command to Panel with CMD 35h - wait pkthdr tx done time out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i. MX8M Mini MIPI-DSI Issue Send DCS Command to Panel with CMD 35h - wait pkthdr tx done time out

2,608件の閲覧回数
mharg
Contributor I

We have a Panel that requires init commands to be sent.

We have modified the panel-raydium-rm67191.c to send our command list.

As with similar questions, we moved sending the command list from the 'prepare' function to the 'enable' function.

Using the 'generic_write' will successfully send all commands. But if we use the 'dcs_write' functions it fails after over 100 commands are sent.

From testing, it appears to be due to sending a command with 0x35 as the cmd field, eg:

 

 

mipi_dsi_dcs_write_seq(dsi, 0xFF,0x30);  // set target to config page 3
mipi_dsi_dcs_write_seq(dsi, 0xFF,0x52);
mipi_dsi_dcs_write_seq(dsi, 0xFF,0x03);
...
mipi_dsi_dcs_write_seq(dsi, 0x35,0x00);  // After this command D0+ & D0- held low
mipi_dsi_dcs_write_seq(dsi, 0x36,0x00);  // This command fails with wait pkthdr tx done time out because it can't transmit while lines held

 

 

(commenting out any 0x35 commands successfully completes sending all commands).


From digging, it appears that the IMX8MM MIPI-DSI controller sees the 0x35 command as the "MIPI_DCS_SET_TEAR_ON = 0x35" command and automatically sets the lines in BTA mode. From the datasheet DSI_ESCMODE register:

mharg_0-1730356220965.png

But we're sending this as a custom register configuration request to the panel, not a SET_TEAR_ON request.

Note: That this issue occurs exactly the same with or without a panel connected.

Is there a way to disable the automatic BTA request when the controller sees a 0x35 command?

 

0 件の賞賛
返信
3 返答(返信)

2,583件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello @mharg 

Referring the MIPI DCS spec, the command 0x35 is set_tear_on.

Zhiming_Liu_0-1730443988446.png

And referring the RM, set_tear_on will set BTA automatically. 

Zhiming_Liu_1-1730444059846.png

 

Is there a way to disable the automatic BTA request when the controller sees a 0x35 command?

-->So we can't disable BTA when the controller sees a 0x35 command

Best Regards,
Zhiming

0 件の賞賛
返信

2,578件の閲覧回数
mharg
Contributor I
Is there a way to cancel or abort the BTA ?
0 件の賞賛
返信

2,546件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

This is a hardware mechanism and cannot be interrupted.

Best Regards,
Zhiming

0 件の賞賛
返信