Hello,
regarding the i.MX8M Mini processor, I cannot find in the documentation (datasheet, reference manual, hardware guidelines) any reference to a fundamental parameter: the characteristic impedance of the GPIO pads depending on the value set in the pinmux control register (DSE bit). Only values such as x1, x2, x4, x6 are indicated, but not in reference to a characteristic R0, as specified for other NXP processors.
I’m experiencing some EMC-related issues on the SDIO lines, and having this parameter would be helpful to potentially test terminations, characterize the line, and perform simulations.
The only thing I found in the datasheet is the current specification at 1.8V and 3.3V under the "GPIO DC parameters," but based on the listed values, I get a minimum value of 1.8V / 9.6mA = 187.5 ohms, which seems extremely high for SDIO signals operating in SDR104 mode (208 MHz)!

Otherwise, I found on page 32 the resistance values for the DDR pads only. I would expect similar orders of magnitude for the SDIO peripheral pads.

IHere there are similar questions I found on the forum:
Solved: iMX8MP drive strength x1..x6 meaning - NXP Community
I.MX8M GPIO output impedance - NXP Community
but the answers are not well explained.. Could someone clarify if I’m missing something?
thank you.