i.MX8M Mini Chromium hardware accelerated issue on Kirkstone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini Chromium hardware accelerated issue on Kirkstone

802件の閲覧回数
Stefano_Radaelli
Contributor I

Hello everyone,

I'm testing Kirkstone yocto release for my i.MX8M Mini board. Using NXP imx-image-full I noticed that Chromium hw accelerated is not working as expected on i.MX8M Mini processor. Every video shown is stuttering and lagging all the time. This is not related to my board because the same happens on IMX8MM-EVK board.
The same image on i.MX8MP, however, is working fine and Chromium is hw accelerated as expected.

Do you have a solution or a workaround for this problem?

Regards,

Stefano

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

786件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you tried with latest kernel version?

If this is not an option, you may refer to the following:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-chromium-hardware-accelerated-vide...

Best regards,
Aldo.

0 件の賞賛
返信

766件の閲覧回数
Stefano_Radaelli
Contributor I

Hello,

thank you for the reply.

I'm using NXP Kirkstone that uses 5.15 kernel.
Thank you for the link, but I think that patch refers to Hardknott with 5.10 kernel, it isn't for kirkstone bsp right?

Regards,

Stefano

0 件の賞賛
返信