i.MX8 X OS container encryption issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 X OS container encryption issue

ソリューションへジャンプ
5,001件の閲覧回数
Joomar
Contributor II

I prepared os_cntr_signed.bin booting well

3 elements are embedded in this container: dtb/linux/rootfs

After encrypting it with cst-3.3.2 the os_cntr_signed.bin cannot boot.

AHAB indicates "Error: authenticate img 2 failed, return -5". SECO Event is 0x0088A929 => A9 Unknown Indicator

Encryption seems ok for img0 and img1 but not for img 2 (rootfs).

In the CST process [Install Secret Key] Image Indexes = 0xFFFFFFFF

is there a restriction with rootfs?

 

0 件の賞賛
返信
1 解決策
4,693件の閲覧回数
Joomar
Contributor II

Hi Hector,

After updating imx-seco >= 3.7.5 that solved the issue.

Thank you for your help

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,915件の閲覧回数
Joomar
Contributor II

Hi Hector,

is it possible to provide previous cst-3.3.1 version to compare?

0 件の賞賛
返信
4,767件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @Joomar ,

I hope you're doing well and sorry for the late reply, I somehow missed this last comment.

Please try using CST 3.4.0 (released today). Search | NXP Semiconductors

The first result in the search should be IMX_CST_TOOL_NEW (just double check that under the file it says Rev 3.4.0). Also, I'd recommend reading the release notes (specially the known issues section). Let me know if this works for you.

Best regards,
Hector.

0 件の賞賛
返信
4,730件の閲覧回数
Joomar
Contributor II

Hi Hector,

Thank you for your help.

Unfortunatly, same issue with cst-3.4.0.

Nothing is mentionned on CST Release note about an eventual rootfs encryption restriction.

The CST off line process is OK but on the target if the Image2 is encrypted that cannot boot.

 

0 件の賞賛
返信
4,699件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @Joomar ,

What errors are being shown when trying to boot image2 (if any are shown)? And how are you flashing said image?

Best regards,
Hector.

0 件の賞賛
返信
4,694件の閲覧回数
Joomar
Contributor II

Hi Hector,

After updating imx-seco >= 3.7.5 that solved the issue.

Thank you for your help

 

0 件の賞賛
返信
4,971件の閲覧回数
Joomar
Contributor II

After encryption the Flags associated to img0 (Flags=0x943) img1 (Flags=0x944) img2 (Flags=0x944)

Testing os container without encrypting img2 only => [Install Secret Key] Image Indexes = 0xFFFFFFFB

Then img0 (Flags=0x943) img1 (Flags=0x944) img2 (Flags=0x144 => no encryption).

In this case the binary boots well.

Why the DEK blob inserted in the binary works well for img0 and img1 ? and not for img2?

Do you have an idea what is wrong?

The RSA key length is 2048 then 3 images should be supported.

 

0 件の賞賛
返信
4,941件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @Joomar ,

I hope you're doing well!

Have you reviewed the following guide from our U-Boot repo? uboot-imx/doc/imx/ahab/guides/sign_os_cntr.txt at lf_v2022.04 · nxp-imx/uboot-imx · GitHub

Also could you confirm exactly the i.MX you're using? And is it a custom board or one of our EVKs?

Thank you.

Best regards,
Hector.

0 件の賞賛
返信