i.MX8 - W21H2-1-4-1-imx-windows-bsp.zip - Run: Init.sh failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 - W21H2-1-4-1-imx-windows-bsp.zip - Run: Init.sh failed

673 次查看
Alex_Chang_633
Contributor III

Hi Teams,

I have questions about BSP source code package.

We follow NXP document to prepare WSL - Ubuntu 20.04 LTS and start to initialize BSP source code packages.

We follow i.MX Windows 10 IoT User’s Guide Page 5 to run Init.sh but it throws error as follows.

i.MX8_BSP_Error_Init.sh.png

 

It will be very helpful, if anyone can give us some advices to solve this problem.

Thanks for NXP Teams help.

0 项奖励
回复
4 回复数

643 次查看
Alex_Chang_633
Contributor III

Hi Teams,

I have download W21H2-1-4-1-imx-windows-bsp.zip from as follows place.

Windows 10 IoT Enterprise for i.MX Applications Processors | NXP Semiconductors

After download was done, I have used tool to calculate file hash as follows:

MD5: c4bcce9bef2f947ed4b69649aea1a306

SHA-256: 451a8d85518227fe513b3848ccd838fd0298d06e8025ab172a4342ed59a98ee1

But running shell script: Init.sh, the situation is the same as follows:

Cloning into '/mnt/d/MyBSP/RSC-IMX8M/W21H2-1-4-1-BSP/mu_platform_nxp/Silicon/ARM/MU_TIANO/ArmPkg/Library/ArmSoftFloatLib/berkeley-softfloat-3'...
Submodule path 'mu_platform_nxp/Silicon/ARM/MU_TIANO/ArmPkg/Library/ArmSoftFloatLib/berkeley-softfloat-3': checked out 'b64af41c3276f97f0e181920400ee056b9c88037'
Submodule path 'uboot-imx': checked out '181859317bfafef1da79c59a4498650168ad9df6'
Patching external submodules ...
Init.sh: 46: Syntax error: "(" unexpected

 

My development environment:

  • Microsoft Windows 10 22H2 19045.4096
  • WSL - Ubuntu 20.04 LTS

Thanks for your help. 

0 项奖励
回复

640 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

You better download the 1.5.0 source. At the same link you sent me, I will report this immediately, thanks for report it.

Regards

 

0 项奖励
回复

644 次查看
Alex_Chang_633
Contributor III

Hi Teams,

Thanks for your quick reply. We will try to download file and try to do it again.

Have a nice day

0 项奖励
回复

646 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This is due to a bad zip installation please erase that zip and download again.

Regards

 

0 项奖励
回复