Use Torizon Core Builder to build imx6ull image for SoM with raw NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use Torizon Core Builder to build imx6ull image for SoM with raw NAND

1,466件の閲覧回数
vgelinski
Contributor I

Hi,

I am pretty new to Torizon OS. I have SoM board that has raw NAND memory. I want to build custom image for it using the Torizon Core Builder. In the Input section I am passing this URL as remote source: "https://artifacts.toradex.com/artifactory/torizoncore-oe-prod-frankfurt/kirkstone-6.x.y/release/8/co.... Note that this is image for eMMC, not for raw NAND. So, as expected I get error while trying to install thie generated image with Toradex Easy Installer. When I connect to the VNC server at 192.168.11.1, I get the following error: Error message
I am getting the download link from this list . But I don't see image for imx6ull board with raw NAND memory. My question is, how do I get a link to the correct image, or how should I modify the tcbuild.yaml config file, so that I get the correct output.


P.s. I have a sample config file for buildroot, and it works. But now I want to try Torizon Core Builder. I can compare the two image.json file - one generated by Buildroot, and one generated by using Torizon Core Builder. So, I know in general how to modify the image.json file, but I don't want to do it manually. In the best case scenario, I should modify only tcbuild.yaml file, and it should generate correct image.json file.

0 件の賞賛
返信
2 返答(返信)

1,464件の閲覧回数
vgelinski
Contributor I

Sorry, image not attached in original post. Here is the error message:
https://ibb.co/d6cJC4F

0 件の賞賛
返信

1,455件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone from @Torizon will help.

Regards

0 件の賞賛
返信