i.MX8 SOC for motor control and NXP RTCESL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 SOC for motor control and NXP RTCESL?

2,396 Views
dmytty
Contributor I

The i.MX8 may be a great control and GUI SOC, combining advanced FOC motor control with technologies like Time Sensitive Networking (TSN) and Machine Vision.  Here's my thinking. 

 

In addition to the powerful A53/A72 main cores co-processor M4 cores, the i.MX8 and i.MX8X also have a Hi4 DSP core and other 'audio interfaces' that may be compatible with 'industrial control'.  While the Tensilica DSP core and IO are designated as 'audio DSP and interfaces', there are similarities between the audio domain and industrial/motor control domain.

The i.MX8 seems to have the necessary hardware.  For example, ADC sample frequencies are at similar frequencies for high RPM motor control and CD/HD audio, and the i.MX8 has 2x ADC with 16 channels at 12 bit (this bit depth is used by other  motor control SOCs).  The i.MX8 also has mechanisms (BootROM, TrustZone?) to allow for guarded code (such as the LineStream SpinTAC libraries).   The i.MX8 M4 cores have 16 KB of L1 and 256 KB of SRAM, while other LineStream SpinTAC compatible SOCs have 12 KB RAM and 32 KB Flash.  The 640+ Mhz HiFi4 DSP has 32/48 KB RAM cache and 64 KB TCM RAM.

 

From a high level, this combination of hardware capabilities means the i.MX8 has the necessary feedback sensors and DSP/M4 control cores exist for doing very powerful stuff.  The 266 Mhz M4 cores included on the i.MX8 are more than fast enough (60 Mhz suffices on other SOCs) and the M4 core is already deployed for the NXP RTCESL: Real Time Control Embedded Software Motor Control and Power Conversion Libraries (Real Time Control Embedded Software Motor Control and Power Conversion Libraries|NXP).  Additionally, the i.MX8X is qualified for SIL 3 industrial application with ECC, EMI and industrial temp ratings. 

 

So...so...SOCs like i.MX8 for industrial/motor control with awesome graphical interfaces and real time networking?  Is there anything that I'm missing that might stand in the way (other than Marketing's Grand Schemes)?

0 Kudos
Reply
3 Replies

2,235 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the i.MX8 is still in pre-production and we do not have enough information about the specification of the product. The most that we had is the information that is on the web-page. However, I recommend you to see the below document, on that document you can find most of the marketing information about the product.

https://www.nxp.com/docs/en/fact-sheet/IMX8FAMFS.pdf 

I apologize for the inconveniences this could give you. 

Best Regards,

Diego.

0 Kudos
Reply

2,235 Views
dmytty
Contributor I

Now that i.MX8 is definitely in production, could you reopen this?

0 Kudos
Reply

2,235 Views
dmytty
Contributor I

Please review and confirm your information.

The i.MX8 and i.MX8X are in pre-production?

The PDF you linked to mentions 'available now' for prototyping:

"EARLY DEVELOPMENT ACCESS The i.MX 8 multi-sensory evaluation kit (MEK)is available now to prototype i.MX 8 and i.MX 8X systems. Contact your NXP sales representative for details."
Could you get someone on the i.MX8 and RTCESL to comment? 
Considering that the last binary release of the RTCESL was 2-3 years ago, I don't think that the only consideration is the shipping schedule of new SOCs.  RTCESL might be dead on all new platforms?  Pity if so.
0 Kudos
Reply