i.MX8 SCU configurations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 SCU configurations

3,444 Views
shabeerbadarudh
Contributor IV

Hi All,

We are using i.MX8 for a new product. Let me help to clear my queries!

1. I have got SC FW APIs doc and "NXP MakeSCD Tool Guide" from freescale community but didn't find the "MakeSCD tool". From where will we get the tool?
2. If we want to assign a peripheral (for example I2C) to M4 core , do we need to assign it using SCI FW API in u-boot or need to configure using  MakeSCD utility.
3. I have seen SC FW APIs in Linux source code also. Does it mean SCI APIs will work on linux and similar OSes(QNX,Integrity etc.)?

Thanks in Advance,

Shabeer

0 Kudos
Reply
3 Replies

2,383 Views
shabeerbadarudh
Contributor IV

Hi Yuri,

Let me know when will be the approximate planned date?

Thanks,

Shabeer.

0 Kudos
Reply

2,384 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, this information also is not available publically.

You may create request or apply to local NXP representative for more information.

Regards,

Yuri.

0 Kudos
Reply

2,384 Views
Yuri
NXP Employee
NXP Employee

Hello,

IMX8 is not supported yet publically.

Regards,

Yuri.

0 Kudos
Reply