i.MX8 RAM specification clarification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8 RAM specification clarification

跳至解决方案
2,710 次查看
pbain
Contributor III

Hi, it appears that there is some difference in the specifications of the RAM capabilities in the i.MX8. Are you able to clarify please?

Document: IMX8QMAEC_Rev. H, page 2 & 6
64-bit LPDDR4 @1600 MHz, 64-bit DDR4 @ 1200MHz

Document: IMX8QMAEC_Rev. H, page 8
2 channels of 32-bit memory
LPDDR4 up to 1.6 GHz
DDR4 up to 1.2 GHz

So are they 64-bit or 32-bit?

Regards,
Peter

标记 (1)
1 解答
2,555 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QM support 64bit LDDR4 and DDR4. There are two channels of 32-bit memory, channel 0 and channel 1, together are 64bit. Hope this can do help for you.

Have a nice day

Rita

在原帖中查看解决方案

3 回复数
2,556 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QM support 64bit LDDR4 and DDR4. There are two channels of 32-bit memory, channel 0 and channel 1, together are 64bit. Hope this can do help for you.

Have a nice day

Rita

2,550 次查看
skuzu
Contributor II

Hi,

I want to check if  i.MX8QuadMax  (or i.MX8QuadPlus) still supports regular DDR4 interface? Or only LPDDR4? 

i.MX8QuadMax / i.MX8QuadPlus datasheets are listing only LPDDR4 and specifiying DDR VDDQ  voltage as Typ. 1.1V, complaint with LPDDR4 spec, but not with regular DDR4.

Is there a way to use regular 1.2V 16-bit DDR4 discrete chips with 8QuadMax or with 8QuadPlus?

thanks,

Selcuk

 

 

 

 

 

0 项奖励
回复
2,555 次查看
pbain
Contributor III

Thank you!

0 项奖励
回复