i.MX8 QuadMax ISO7816 implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 QuadMax ISO7816 implementation

ソリューションへジャンプ
3,450件の閲覧回数
Vlatakomarac
Contributor II

Hello,

I have a carrier board that contains an i.MX8 QuadMax processor.

I want to connect a SAM card slot to this processor but the manufacturer didn't make physical lines on the carrier board so a connection can be made between the SAM card and the integrated SIM module of the i.MX8 QuadMax (pins SIM0_CLK, SIM0_IO and so on).

Does anyone know how can I implement ISO 7816 communication with a running Linux OS on the i.MX8 processor without using the Linux drivers which use the SIM module?

I would appreciate any kind of help. Thank you in advance!

ラベル(1)
0 件の賞賛
返信
1 解決策
3,443件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nikola

 

>how can I implement ISO 7816 communication with a running Linux OS on the

>i.MX8 processor without using the Linux drivers which use the SIM module?

 

I am afraid this is not possible, sorry. In general one can try simple sim unit test

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_sim_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

元の投稿で解決策を見る

4 返答(返信)
3,444件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nikola

 

>how can I implement ISO 7816 communication with a running Linux OS on the

>i.MX8 processor without using the Linux drivers which use the SIM module?

 

I am afraid this is not possible, sorry. In general one can try simple sim unit test

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_sim_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

3,433件の閲覧回数
Vlatakomarac
Contributor II

Thank you Igor on your reply.

It is good to know if it is feasible or not so thank you.

What did you mean by using the sim unit test? What would be the goal of running this test?

0 件の賞賛
返信
3,429件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>What would be the goal of running this test?

 

test basic sim functionality.

 

Best regards
igor

0 件の賞賛
返信
3,420件の閲覧回数
Vlatakomarac
Contributor II

I have been looking for a solution to the problem.

The only solution that I see is to use another microcontroller from the PN7462 family. They have integrated ISO UART modules, but this complicates the design because now there is another uC to program.

Could you recommend another IC that possibly implements ISO 7816 protocol but doesn't need to be programmed? I would use a TDA8037 but it requires that the uC implements the ISO 7816.

Thank you again. Best regards.

0 件の賞賛
返信