i.MX8 PLUS expand memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 PLUS expand memory

4,335 Views
synwzh
Contributor I

Hi,

I Would like to consult i.Mx8 series chip support external expansion of LPDDR4 and emmc, such as MIMX8QX6AVLFZAC.

Looking forward your reply, thank you

0 Kudos
Reply
7 Replies

4,309 Views
bixby6245
Contributor I

Hello

The i.MX8 PLUS processor supports expandable memory options through the use of external memory interfaces such as DDR or LPDDR. To expand the memory of an i.MX8 PLUS device, the user must connect an external memory module to the device's memory interface. The external memory module must be compatible with the i.MX8 PLUS memory interface specifications and should be purchased from a trusted source.

Before purchasing a memory module, the user should consult the i.MX8 PLUS datasheet for the device's memory interface specifications and requirements. Once the memory module is connected, the user can configure the device to use the additional memory through the device's software or firmware.

 

Dinar Guru

0 Kudos
Reply

4,298 Views
synwzh
Contributor I

Hello bixby6245,

Thanks for your reply. I would like to know whether there is a limit on DDR capacity besides interface compatibility.

 

0 Kudos
Reply

4,312 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @synwzh,

I hope you are doing well.

i.MX8QXP supports LPDDR4 with maximum density of 4GB.

Since the i.MX8QXP is compliant with eMMC System Specification v5.1, it supports up to 128GB density for eMMC as per standard specifications.

Thanks & Regards,
Ritesh M Patel 

0 Kudos
Reply

4,300 Views
synwzh
Contributor I
I have found the LPDDR4 evk board on the nxp official website, which uses MIMX8ML8DVNLZAA +  6 GB LPDDR4(Micron MT53E1536M32D4DT-046 WT:A),Which chip has the largest DDR capacity supported by imx8 series and how much memory is supported.
 
By the way, does imx8 series have naming rules similar to the ones shown in the picture below? Can you provide them?
synwzh_4-1675303205245.png

 

Thanks,

Zhihua

 
0 Kudos
Reply

4,292 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @synwzh,

One can refer to the below link which lists all processors from i.MX8 series.

One can select the best candidate based on the requirements.

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

4,288 Views
synwzh
Contributor I

Hi @riteshmpatel 

Thank you for your reply,I got the link,and another question “You told i.MX8QXP supports LPDDR4 with maximum density of 4GB,but I have found the LPDDR4 evk board on the nxp official website, which uses MIMX8ML8DVNLZAA +  6 GB LPDDR4(Micron MT53E1536M32D4DT-046 WT:A),Which chip has the largest DDR capacity supported by imx8 series and how much memory is supported.”

Thank you

0 Kudos
Reply

4,285 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @synwzh,

i.MX8QXP and MIMX8ML8DVNLZAA are both different processor from i.MX8 series.

Please refer to the above-shared link. One can refer to the Reference Manual of each processor for max memory support.

Thanks & Regards,
Ritesh M Patel

 

0 Kudos
Reply