i.MX8 Mini JTAG Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 Mini JTAG Interface

1,836件の閲覧回数
shawnnageli
Contributor II

Looking at the schematics for the 8MMINILPD4 base board design JTAG interface to the processor I am curious about the functionality and purpose of diodes D907 and D908.  Are these used to to control the nRST and keep the JTAG from overriding POR_B?  I have the snapshot from the schematic showing the diodes in question.

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,661件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

So sorry for late reply. I have confirmed it for you. The power domain of POR_B is VSNVS, the power domian of Jtag IO is DCDC_3V3. External Jtag device output nRST signal to our system, its power domain is different our system. So D1905 and D1906 is for isolation of different power domain, in order to keep the current from flowing back.

Hope this can do help for you.

Have a nice day

Best Regards

Rita

0 件の賞賛
返信