i.MX8 Mini EVK Bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 Mini EVK Bluetooth

7,919件の閲覧回数
IRENE_U
Contributor I

In the i.MX8 Mini EVK which just bought without doing anything, and using your OS which had already burn in the NAND FLASH.

I have seen the BT icon in the system,but why the BT function cannot be use? 

Thanks

0 件の賞賛
返信
6 返答(返信)

7,910件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you use nxp imx8mm ddr4 board? which bsp version do you use?

 

0 件の賞賛
返信

7,892件の閲覧回数
IRENE_U
Contributor I

Yes, I use imx8mm DDR4 EVK, and it show "Unavailable" on BT address.

Andriod 9

Kernel version :4.14.98-00063-gbcdaf61 #1 Sun Apr 7 02:27:35 CST 2019

 

0 件の賞賛
返信

7,886件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you send me the picture of "Unavailable" ? I flashed the P9.0.0_2.0.0 images to the IMX8MM DDR evk SD card, doesn't have the same issue as yours, refer to the schematic and user guide, The BCM 1MW Wi-Fi/Bluetooth module is used on the i.MX 8M Mini EVK DDR4 Board.

0 件の賞賛
返信

7,810件の閲覧回数
IRENE_U
Contributor I

Besides, I tried to use command "rfkill" to open BT through debug port.

But It shows nos such command.

Is there any solution ?

Thanks.

0 件の賞賛
返信

7,874件の閲覧回数
IRENE_U
Contributor I

You can see that wifi is OK, but BT doesn't show my device ID and can't find other device.

DSC_1641.JPG is before connectint to wifi.

DSC_1644.JPG is after connectint to wifi.

0 件の賞賛
返信

7,714件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what android 9 do you need to use? I need to download the source code to check if current bsp enable it or not

0 件の賞賛
返信