i.MX8 Family Performance comparisons ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 Family Performance comparisons ?

4,075件の閲覧回数
Ken_Edwards
Contributor I

Looking for a performance comparison for the i.MX8 family of processors, specifically between the i.MX8 QuadPro and the i.MX8 QuadMax.  Ideally standard numbers.

ラベル(1)
0 件の賞賛
返信
1 返信

4,068件の閲覧回数
b36401
NXP Employee
NXP Employee

We have no official performance measurements for these processor.
Theoretical average Dhrystone results for our ARM architectures should be around 2.24 DMIPS/MHz for A53 cores and 4.72 DMIPS/MHz for A72 cores.
Unofficially we measured the performance and got up to 2.85 DMIP/MHz (with best optimization) and up to 5.35 DMIPS/MHz for A72 i.MX8 cores.
And you can see that i.MX8QM has 4 A53 @1.2 GHz plus 2 A72 @1.6 GHz and i.MX8QP has 4 A53 @1.2 GHz and 1 A72 @1.6 GHz.

0 件の賞賛
返信