i.MX7D application without DRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D application without DRAM

1,053件の閲覧回数
chris_f
Contributor V

Is it possible to use the iMX7D without any DRAM? NVCC_DRAM is required ON in the RUN mode according to IMX7DCEC table 14. Will the device enter RUN mode without this? If NVCC_DRAM is required, does there actually need to be any DRAM attached to enter RUN mode?

ラベル(1)
0 件の賞賛
返信
1 返信

978件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 It is possible to use the iMX7D without any DRAM, at least in theory,

when user applications do not require much memory. Usually it is

bare metal codes, working without OS support.

  In any case i.MX7 NVCC_DRAM must be applied.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信