Greetings,
I work with i.MX7 Dual module and try to enable a SecureBoot feature. All worked well for i.MX7 SoC of Rev 1.2, but after switching to SoC of Rev 1.3, a strange HAB event, which makes SecureBoot fail, started to appear:
=> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x22 0x33 0x00
0x00 0x00 0x00 0x0f 0x00 0x91 0x00 0x00
0x10 0x00 0x00 0x00
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_TARGET (0x33)
ENG = HAB_ENG_ANY (0x00)
=>
I've googled for this problem and found similar issues on this forum:
https://community.nxp.com/t5/i-MX-Processors/iMx7D-HAB-Event-issue/m-p/912400
https://community.nxp.com/t5/i-MX-Processors/HAB-loading-to-OCRAM-and-software-update/m-p/972771
And it seems that some solution has been privately provided by NXP employees to the authors of these topics. If it's possible/allowable, could you please share it with me as well?
Additional information about my configuration:
- Freescale i.MX7D rev1.3 1000 MHz (running at 996 MHz)
- U-Boot 2021.04 (but the same issue can be observed on lf-6.1.1-1.0.0 NXP release)
- SPL is used, which is booted from on-board SPI flash.
Please tell if additional information is needed.
Best regards,
Mikhail.
解決済! 解決策の投稿を見る。
Hi @mikhail_vanylin ,
I hope you're doing great! Please check the email I've sent with additional information regarding your case.
Thank you.
Best regards,
Hector.
Hi @mikhail_vanylin .
I hope you're doing well. Let me review if we have that available to share.
Thank you.
Best regards,
Hector.
Hi Hector @hector_delgado,
thanks for the feedback! Looking forward for news from you.
Please tell if additional information about me or my organization is needed. Or I can ask my customer, who should have some direct contact/agreement with NXP to reach you privately about this problem. We can continue this discussion in private mode.
Best regards,
Mikhail Vanylin.
Hi @mikhail_vanylin ,
I hope you're doing great! Please check the email I've sent with additional information regarding your case.
Thank you.
Best regards,
Hector.