i.MX7D SDMA for mem-to-ext peripheral transfers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D SDMA for mem-to-ext peripheral transfers?

ソリューションへジャンプ
1,133件の閲覧回数
thomasdoerfler
Contributor II

Hi,

I intend to use the i.MX7D SDMA engine to transfer a byte stream from system memory (DDR RAM) to an FPGA attached to the EIM. The FPGA should be able to trigger transfers using DRQ lines.

I have the SDMA up and running for mem-to-mem transfers (using the ap_2_ap script), but I still have two challenges:

- the SDMA should not increment the destination (FPGA) address from one byte to the next

- each byte should be triggered with the external event (DRQ line)

For i.MX6, there seems to be a ap_2_ap_fixed script, but I don't see it documented for the i.MX7.

Any hints?

0 件の賞賛
返信
1 解決策
1,114件の閲覧回数
ceggers
Contributor V

Hi Thomas,

I have created tools (binutils port + plugin for Lauterbach Trace32) for developing and debugging custom SDMA scripts. It seems that you are already familiar with the basics of the SDMA, so you could easily modify the existing scripts for your need.

Alternatively I can do the necessary customization for you. I should be able to do this within a few days.

Please contact me directly (German preferred )  for more details.

regards
Christian

元の投稿で解決策を見る

3 返答(返信)
1,115件の閲覧回数
ceggers
Contributor V

Hi Thomas,

I have created tools (binutils port + plugin for Lauterbach Trace32) for developing and debugging custom SDMA scripts. It seems that you are already familiar with the basics of the SDMA, so you could easily modify the existing scripts for your need.

Alternatively I can do the necessary customization for you. I should be able to do this within a few days.

Please contact me directly (German preferred )  for more details.

regards
Christian

1,084件の閲覧回数
thomasdoerfler
Contributor II

Christian,

this really sounds interesting. Having an adapted script with the required functionality enables the SDMA to fulfill its purpose in my application.

Thanks a lot!

0 件の賞賛
返信
1,119件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi thomasdoerfler

 

I am afraid such script is not available (not "officially" supported), sorry.

One can try to develop custom script using tutorial : http://billauer.co.il/blog/2011/10/imx-sdma-howto-memory-map/

or with Professional Services: https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 件の賞賛
返信