i.MX7 Kernel Config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 Kernel Config

2,379 Views
ryanschaefer
Contributor IV

Linux Kernel v4.9.11_1.0.0_ga commit 427eb83 fails to build when only configured for IMX7D SOC. A diff for the kernel configuration patch as attached. Putting this here because the imx kernel repository has no public facing issue tracker.

gcc version 7.3.0

Compiler Output:

drivers/built-in.o: In function `imx7d_charger_primary_detection':
core.c:(.text+0x24df58): undefined reference to `bq2429x_set_ilim'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_pre_suspend':
platform-imx-dma.c:(.text+0xf5c): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0xf68): undefined reference to `imx_gpc_enet_wakeup_enabled'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_post_resume':
platform-imx-dma.c:(.text+0x10d0): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0x10dc): undefined reference to `imx_gpc_enet_wakeup_enabled'
Makefile:969: recipe for target 'vmlinux' failed
make: *** [vmlinux] Error 1

Thanks,

Ryan

EDIT:

Building also fails if config option CONFIG_ARM_IMX6Q_CPUFREQ is not set. This should also be fixed.

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

1,983 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ryan,

Can you please share the link of the git repository where you fetch to download the committ that you are mention?.

0 Kudos
Reply

1,984 Views
ryanschaefer
Contributor IV

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/log/?h=imx_4.9.11_1.0.0_ga 

The commit I shared is the head of freescale provided linux git repository branch imx_4.9.11_1.0.0_ga. I agree that NXP's kernel repositories are not friendly and should be unified.

0 Kudos
Reply