Hi Team,
This is regarding our project TOYOTA_MEUCY17 based on i.MX6 Quad and based on L3.10.17_1.0.2 release. This project uses X11.
In one of our use case browser application is crashing when Coyote app is running and it crashes only when eglCreateWindowSurface returns EGL_BAD_ALLOC. This is sometime issue and not reproducible each time. Looking at the callstack from coredump file it points towards the GPU driver. Please check the attached complete call stack and snapshot from it below.
In logs we are observing following logs:
meucy17-t101-a0 [ 3] ERR_BREAK: status=-1(gcvSTATUS_INVALID_ARGUMENT) @ _CreateSurfaceObjects(584)
meucy17-t101-a0 [0411/063012:ERROR:gl_surface_egl.cc(410)] eglCreateWindowSurface failed with error EGL_BAD_ALLOC
meucy17-t101-a0 [0411/063012:ERROR:command_buffer_proxy_impl.cc(155)] Failed to initialize command buffer service.
meucy17-t101-a0 [0411/063012:ERROR:webgraphicscontext3d_command_buffer_impl.cc(213)] CommandBufferProxy::Initialize failed.
meucy17-t101-a0 [0411/063012:ERROR:webgraphicscontext3d_command_buffer_impl.cc(230)] Failed to initialize command buffer
Could you please help us in resolving this issue.
Regards,
Ikshwaku
Hello,
L3.10.17_1.0.2 release is very old bsp, using gpu 4.x. Gpu is 6.x now. Our team no longer support it. The support request should go to NXP professional software service.
Professional Support for Processors and Microcontrollers | NXP
Regards
Hi ikshwaku.chauhan,
Are you using Linux system based on Yocto BSP L3.10.17_1.0.2? If yes, can you let us know how did you integrated coyote application in Yocto?
Regards,
Kunal
Hello Kunal,
Yes we are using Yocto BSP L3.10.17_1.0.2 and coyote app is a HTML based java script that uses Chromium Browser provided apis. And browser internally calling all X11 and graphics specific calls.
So, here coyote app is just a script.
Regards,
Ikshwaku
Hello Ikshwaku,
Set default bpp to 16, Similar issue was solved at:
EGL eglCreateWindowSurface issue 3.14.28
You have to update your bsp a lot of bugs are fixed in latest release L4.14.88 .
Hi,
eglCreateWindowSurface returns EGL_BAD_ALLOC in following condition:
If there is already an EGLSurface associated with native_window
Or
implementation cannot allocate resources for the new EGL window
We explored about this error and found that this seems to be application specific issue.
This error occurs when the application try to create eglWindowSurface but the previous window has not been destroyed yet. In application side we can keep error check that will verify if previous eglWindowSurface has been destroyed and only after that call to eglCreateWindowSurface is execute.
Let us know in case the issue persist even after changing the application
Regards