i.MX6q Sabre SD : boot from SPI NOR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6q Sabre SD : boot from SPI NOR

3,630 Views
GabrielHuau
Contributor I

Hi,


I'm trying to boot from the SPI NOR with the i.MX6 Sabre SD. I'm able to boot from the eMMC and SD slot, but when I flash the NOR with u-boot at 0x400, boot switch 6 and 7 are set to "1" and others to "0", I'm not able to start u-boot. I tried with the i.MX6q Sabre Lite, and no problems (but no switch to configure the boot mode).

Someone succeed to boot from SPI NOR with the Sabre SD ?

Best regards,

0 Kudos
Reply
3 Replies

3,021 Views
Poussemousse
Contributor III

Hello Gabriel,

Do you manage to boot from the SPI NOR with i.MX_6DualLite_Sabre-SDP Platform?

If so, can you  explain me how?

Best regards.

0 Kudos
Reply

3,021 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Sorry, seems like the table was cut when uploaded. I'm attaching the file with the complete table.

 

Best regards.

Jorge.

0 Kudos
Reply

3,021 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Gabriel,

 

Are you trying to boot from U50? If so, please try the following configuration in SW40, SW39 and SW36.

 

SW37 and 38 don't have influence in this case, so you can configure them however you want.

 

 BT_MODE0BT_MODE1BT_CFG1_7BT_CFG1_6BT_CFG1_5BT_CFG1_4BT_CFG1_3BT_CFG1_2BT_CFG1_1BT_CFG1_0BT_CFG4_7BT_CFG4_6BT_CFG4_5BT_CFG4_4BT_CFG4_3BT_CFG4_2BT_CFG4_1BT_CFG4_0
 SW40_1SW40_2SW39_8SW39_7SW39_6SW39_5SW39_4SW39_3SW39_2SW39_1SW36_8SW36_7SW36_6SW36_5SW36_4SW36_3SW36_2SW36_1
SPI NOR010011XXXXXX000000
                   
X = Don't care                  

 

Best regards.

Jorge.

0 Kudos
Reply