i.MX6ULL DDR3L Script Aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL DDR3L Script Aid

4,279 Views
viralvasa
Contributor I

Hi Team

    I am using DDR test tool v3.0. I wanted to run the calibration test for Memory density - 1GB ( Micron - MT41K512M16VRN-107 IT:P) . The problem statement is I don't have script file to be loaded for this configuration. can any one provide proper script file for below configuration:

- 1GB memory density

- DDR operating freq is 400 MHz

- DRAM bus width is 16

Please provide the script file .inc for me to run the calibration. 

Labels (2)
0 Kudos
Reply
5 Replies

3,940 Views
jochenstehle
Contributor III

Hello,

did you have a linux running with die MT41K512M16VRN?

We tried it but the kernel didnt start. Only if wie set the DRAM size to 800MB the Kernel start.

0 Kudos
Reply

3,940 Views
viralvasa
Contributor I

Thank You very much Yuri, This setting worked for me. 

0 Kudos
Reply

3,940 Views
viralvasa
Contributor I

Hi Yuri 

  Thank you very much for reply. 

  I already have this tool, but I need to load a script file for 1GB memory. to do calibration. 

  is my understanding right that script file is needed for different density memory ? current tool has script file of max 512MB only.  can you please let me know on this issue

0 Kudos
Reply

3,940 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please try the following settings.

pastedImage_1.png

Regards,

Yuri.

0 Kudos
Reply

3,940 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Customers can use the following tool:

“i.MX6ULL_DDR3_Script_Aid”

https://community.nxp.com/docs/DOC-333791

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply