i.MX6ULL CSI/GPIO Set

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL CSI/GPIO Set

5,897 Views
lizboxy
Contributor I

Now,we use i.MX6ULL‘pin  of csi_data06 and csi_data07 as GPIO.

So how can I set the resiter of  IOMUXC_SW_PAD_CTL_PAD_CSI_DATA06 and IOMUXC_SW_PAD_CTL_PAD_CSI_DATA07 in linux?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

3,929 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

gpio example for these pads can be found in

linux/imx6ull-colibri.dtsi at master · torvalds/linux · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply