i.MX6UL platform on Windows 10 IoT embedded system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL platform on Windows 10 IoT embedded system

1,949 Views
adamhuang
Contributor III

Since we have finished a project based on i.MX6UL which was developed in YoctoProject environment, we will like to study whether there is possibility to develop it with Windows 10 IoT Core. Prier to study, there are several questions that should be clarified first.

(1) Is Windows 10 IoT free? Should we pay for the license? How much is it?
(2) Is it easy to integrate the present opensoftware into Windows10 IoT? (Such as Net-SNMP, SSHD etc)

(3) Can it be specified to a specific 3rd-party Cloud Sever as our potential customer desire to connect the edge devices?

Best Regards

Labels (2)
0 Kudos
Reply
2 Replies

1,441 Views
reylandzoren
Contributor I

Great article. I want to thank you for your advice.

0 Kudos
Reply

1,850 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Adam,

For all your questions you can check:

Overview of Windows 10 IoT Core - Windows IoT | Microsoft Docs 

Regards

0 Kudos
Reply