i.MX6UL SNVS current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL SNVS current

2,238 次查看
TammyTsai
Contributor III

Hi NXP team,

I would like to ask a question about the Battery Backup current.

The current of VDD_SNVS_IN of i.MX6UL will reach up to 500 uA.

Even if TAMPER PINs are not used, it will still be 205uA.

Using a CR2450 battery (about 550 mAh), such current consumption will run out of power in 2 months.

Products from other manufacturers have a maximum of around 20uA, or even less than 10uA.

image004.pngimage006.pngimage008.pngimage010.pngimage015.png

Does NXP have any improvement plans or other suggestions for battery backup?

 

Best Regards,

Tammy

标签 (1)
0 项奖励
回复
3 回复数

2,191 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @TammyTsai,

I hope you are doing well.

Please refer to the latest i.MX 6UltraLite Power Consumption Measurement Application Note. The current consumption in the SNVS domain is 22uA as mentioned in Table 10. SNVS measurement results. Apart from this, no other data is available.SNVS.PNG

 I hope it helps!

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复

2,079 次查看
TammyTsai
Contributor III

Hi @riteshmpatel,

Thanks for your reply.

TammyTsai_0-1696569480888.png

How to address the BOOT_MODE requirement of step 2?

Could I switch BOOT_MODE by software?

Could you please described the method in detail?

 

Best Regards,

Tammy

0 项奖励
回复

2,072 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @TammyTsai,

I request you to please raise a new ticket for the additional query.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复