i.MX6UL HAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL HAB

2,112件の閲覧回数
ranjithhebbar
Contributor II

Dear all,

 

     I am working on i.MX6UL based custom board. Booting SPL and u-boot-ivt.img normally.

     In HAB case, we signed SPL image and u-boot-ivt.img we tested in Open mode gives "NO HAB Event Found" Message for Authentication. Then we tried HAB closed mode.

   

     In HAB  closed mode, SPL signed image and u-boot-ivt.img signed image will work successfully. And according to document corrupting signed images like SPL-signed-pad.bin and u-boot-signed.img will not boot as expected.

    But Normal images are booting SPL and u-boot-ivt.img (which is not signed) without any error in HAB closed mode. Is this behavior expected in HAB? I am just wondering why normal images are booting..!!!! ?

Best Regards,

Ranjith Hebbar

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,918件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Some HAB features are described in section 4.1.1 (SRK HASH and HAB events in open mode)

of app note AN4581, Rev. 2, 05/2018.

  

https://www.nxp.com/docs/en/application-note/AN4581.pdf 

Regards,

Yuri.

0 件の賞賛
返信

1,918件の閲覧回数
art
NXP Employee
NXP Employee

Yes, this is the expected behaviour. An unsigned image boots successfully even in HAB enabled mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信