i.MX6UL CSI camera preview unit test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL CSI camera preview unit test

1,780 Views
m_c
Senior Contributor I

Where can we find unit test of i.MX6UL CSI camera preview?

gstreamer command is good as below.

gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw,width=640,height=480,framerate=(fraction)30/1' ! imxv4l2sink

However, customer needs simple example code for i.MX6UL CSI camera preview as base for image recognition application. We try several as below doesn't work.

pxp_test.out

pxp_v4l2_test.out

mxc_v4l2_tvin.out

Labels (3)
0 Kudos
Reply
2 Replies

1,411 Views
eric_kang
Contributor II

Dear All,

I'm finding the OV5640 Camera module using Parallel CSI Interface for i.MX6UL.

Firstly I could find the recommended Camera in i.MX6UL EVK Users Guide like as below.

CMOS module : OV5640-MRFL-AB0T / Connector : FX12B-40P-0.4SV

But I couldn't find the Camera module and the compatible camera.

Please let me know where I can buy the Parallel CSI Camera for i.MX6UL-EVK.

Best Regards,

Eric.

0 Kudos
Reply

1,411 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

one can try unit test program mx6s_v4l2_capture.out, with imx6ul-14x14-evk-csi.dts:

$ /unit_tests/mx6s_v4l2_capture.out -d /dev/video1 -m 1 -of 320x240.yuyv

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply