i.MX6UL Battery Backup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL Battery Backup

1,344件の閲覧回数
danielfield
Contributor I

I'm doing a design with the i.MX6UL processor with a coin cell backup for RTC and am needing to draw as little current as possible when there is no system power. 

Using the eval board for this processor, I'm seeing the current draw at 300 uA when powered from VDD_COIN_3V.  I'm assuming this large current draw is coming from various leakage currents on the design:

 - POR_B leakage current on the reset circuitry

 - PMIC_ON_REQ leakage current 

I'm assuming if I use MOSFET's to help isolate these lines during a coin cell only power I can get my coin cell current draw significantly lower?  Are there other areas of leakage current I should be concerned about?

ラベル(1)
0 件の賞賛
返信
1 返信

1,248件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

leakage may be caused by some pads which are powered by VSNVS,

this is  described in Table 10. Power and decoupling recommendations

Hardware Development Guide for the i.MX 6UltraLite Applications Processor
http://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信