i.MX6SoloX NVCC_RGMII voltage setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SoloX NVCC_RGMII voltage setup

1,885件の閲覧回数
tbrisebois
Contributor I

We are using the newer i.MX6SoloX device in our design and looking for some help on the NVCC_RGMII1/2 power groups supplies.

From what I read, these two groups are essentially powered by the PHY that is connected to the i.MX device.  The operating range of NVCC_RGMII is given as 1.35V to 3.6V in table 10 of the IMX6SXIEC. However, there are three “modes” defined for RGMII: 1.5V, 1.8V and 2.5V. Is there anything that would prevent me from supplying 3.3V to this interface? This would make Ethernet connectivity much simpler, and eliminate the need for two separate voltage rails on this interface.

Thanks

tB

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,649件の閲覧回数
art
NXP Employee
NXP Employee

Typically, the RGMII Gigabit Ethernet PHY interface provides an analog voltage regulator (typically, installed on PHY IC) that makes the appropriate supply voltage for the PHY (and corresponding CPU interface) I/O signals. The typical values of this voltage (depending on implementation) are 1.5V, 1.8V or 2.5V. Powering the whole interface from 3.3V may get it out of spec. For example, please refer to the schematics of the i.MX6SoloX SABRE SD board, available on the Freescale web site:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,649件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi TB,

     For RGMII powre, most of PHYs are 1.5V, 1.8V & 2.5V, so datasheet gives 3 kinds of voltage mode. due to the rating of RGMII is 3.6V, so if you use 3.3V for RGMII power, it is no problem.

Regards,

Weidong

0 件の賞賛
返信