i.MX6SDL IDMAC setting for de-interlacing.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL IDMAC setting for de-interlacing.

1,706件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6S IPU IDMAC.

They want to use VDIC de-interlacing processing, but it has not worked well.

Then, we are checking IDMAC setting.

[Q1]

Please see Table 38-29 in IMX6SDLRM Rev.2.

For de-interlacing, IDMAC_CH_5, 9, 10, and 13 should be enabled.

Next, please see Table 38-9, ch 8 seems to be also needed not only ch 5, 9, 10, and 13.

Should we enabled ch 8 also?

[Q2]

Actually, ch 0 in Table 38-9 is enabled now.

To use VDIC de-interlacing, should we disable ch 0 to prevent collision?

Or we can ignore it?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,572件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

Pls refer to the Table 38-30. IPU's Processing flows:

Interlaced input coming from the memory via 3 channels 8, 9 and 10.

so channel 8 is useful. for more detailed information, you can refer to this table ,and you can refer to the source code in the unit test, name includs "tvin".

1,572件の閲覧回数
satoshishimoda
Senior Contributor I

HI Guanqiong Xie,

Thank you for your reply, and sorry my information for your was not sufficient.

Our partner is using CSI -> VDIC -> Mem path with the setting written in the following post.

i.MX6 CSI -> VDIC path

According to your reply, channel 8 is useful for Mem -> VDIC -> Mem path.

But it is not useful for CSI -> VDIC -> Mem path since Table 38-29 does not mention channel 8, right?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信