Hi,
I have built a Linux 3.0.35 kernel for a LCD. At the beginning, there was a correct display on the LCD. However, after setting up an SD/MMC card by using MFGTool or Linux Host for several times, the display on the LCD is wrong, while using the same u-boot, uImage and file system. The final image on the LCD is the image with four penguins on the top left corner.
Here is the bottom of the terminal output.
starting pid 1392, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
udevd (1401): /proc/1401/oom_adj is deprecated, please use /proc/1401/oom_score_
adj instead.
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
BusyBox v1.20.2 () multi-call binary.
Usage: mount [OPTIONS] [-o OPTS] DEVICE NODE
Mount a filesystem. Filesystem autodetection requires /proc.
-a Mount all filesystems in fstab
-r Read-only mount
-w Read-write mount (default)
-t FSTYPE[,...] Filesystem type(s)
-O OPT Mount only filesystems with option OPT (-a only)
-o OPT:
loop Ignored (loop devices are autodetected)
[a]sync Writes are [a]synchronous
[no]atime Disable/enable updates to inode access times
[no]diratime Disable/enable atime updates to directories
[no]relatime Disable/enable atime updates relative to modification ti
me
[no]dev (Dis)allow use of special device files
[no]exec (Dis)allow use of executable files
[no]suid (Dis)allow set-user-id-root programs
[r]shared Convert [recursively] to a shared subtree
[r]slave Convert [recursively] to a slave subtree
[r]private Convert [recursively] to a private subtree
[un]bindable Make mount point [un]able to be bind mounted
[r]bind Bind a file or directory [recursively] to another locati
on
move Relocate an existing mount point
remount Remount a mounted filesystem, changing flags
ro/rw Same as -r/-w
There are filesystem-specific -o flags.
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
starting pid 3128, tty '': '/etc/rc.d/rc_gpu.S'
/etc/rc.d/rc_gpu.S: line 6: /sys/module/galcore/parameters/gpu3DMinClock: No suc
h file or directory
starting pid 3134, tty '': '/etc/rc.d/rc_mxc.S'
arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/
10 09:20) 4.6.2 20110630 (prerelease)
root filesystem built on Fri, 28 Feb 2014 20:05:30 +0800
Freescale Semiconductor, Inc.
freescale login:
Can anybody help me to get an correct display on LCD?
解決済! 解決策の投稿を見る。
Thanks for the information. The uboot, uImage and file system have been downloaded successfully. And the setting of uboot environment is right.
Finally, it is ok when I download file system from rootfs.ext2 in the L3.0.35_4.1.0_130816_images_MX6 instead of from the rootfs folder in ltib folder.
Hi Zeng,
Have you download the uboot, uImage and file system to your board succeed ? And if the setting of uboot environment is right. Would you please check?
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the information. The uboot, uImage and file system have been downloaded successfully. And the setting of uboot environment is right.
Finally, it is ok when I download file system from rootfs.ext2 in the L3.0.35_4.1.0_130816_images_MX6 instead of from the rootfs folder in ltib folder.
Hi zeng,
I recommend you to create the thread in right place i.MX Community, so you can get quick response.
Best Regards
Dan